Use the linux -sdk6.0 software, I want to run linux from MMC0/SD on my own designed board with AM3357, which has only SD and DDR3. However, the linux kernel cannot run , stuck at Uncompressing Linux... done, booting the kernel. Meanwhile, the linux kernel can run successfully on the development board which has SD,DDR3 and NANDflash.