Hello,
I'm planning to buy TMDSEVM6657LS multicore DSP board to interface it with i2c/spi sensors and do complex math operations. The final output of the project is a small board containing the DSP and sensors, However I can notice that the evaluation board is quite large in size for my applications. So, here is my questions:-
1) What are the minimum required hardware on the board to make the DSP work with i2c/spi sensors, one GPIO interrupt, and few LEDs?
2) What is the need to the on-board FPGA in the evaluation board? will I need this FPGA to be implemented on my PCB to be able to control GPIO, sensors...etc?
I will be very grateful if you can answer my simple questions and help me choosing the correct HW.