Hi Travis or other expertise,
I'm looking into the SRIO configuration on C6657/6655, and I need some clarifications on SYS_CLK selection.
Travis said that there is an undocumented register bit or SYS_CLK selection in the following thread.
https://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/282116/992518
Bit 9 of RIO_PER_SET_CNTL1 controls this as the following:
‘0’ => Used SYS_CLK_SEL to define the clock source SYS_CLK
‘1’ => Use vbusp_clk as the clock source for SYS_CLK
Again, this bit is only valid on rev2.0 silicon and reserved otherwise.
I believe this undocumented register bit is valid on C665x silicon rev1.0 as well as C667x silicon rev2.0 - right ?
Thanks,
Sei Kato