Hello I am writting my Thesis and i am
looking for a small system that could merge two camera images and show the whole to a display.
first i would like to give you more informations about the cameras : Cam1 (768 X 578 25
Hz/Cameralink and BNC) + Cam2 (768 X 288 25 Hz/Cameralink and BNC) + Display
(800 X 600 60Hz/VGA).
Could someone here tell me which Board or development Kit or microcontroller i can use to realize this application?
Thank you!
Blaiso