This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue while capturing 1280x960 using ipnc rdk 3.8

Our sensor is connected via the parallel interface to DM8127.

The sensor is configured to output 1280x960@30.

ISS ISP Configuration:

VP--1280x960--->IPIPEIF---->ISIF---->IPIPEIF------>IPIPE------>RSZ---->RSZA:640x480, RSZB:1024x768

Using this setup we couldn't get the output from the resizers(no resizer DMA interrupts appeared) even though
the interrupts from ISIF were arriving for every frame. When we changed our sensor output to1280x962@30
everything seemed to work properly.

The current sensor we are working with is capable of maximal output of 1280x960, meaning we cannot capture
the video.

Please help,

Tal.