This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Processor SDK Linux Release 2.0.0 with Beaglebone

HI,

can i create a bootable sd card for the beaglebone board with this sdk ? Until now i was not able to succeed. If it would be possible how to add support for a LCD ?

We have also currently an am335x evm board with a 7" lcd for testing. What to do if we would take a different lcd ?

Is there support for spi slave mode ? Either in the am335x evm or for the beaglebone board ?

Regards

Erich