Other Parts Discussed in Thread: OMAP-L138, OMAPL138, SYSBIOS
Hi,
For the past three days I have been trying to make my application boot-able on the LCDK-C6748 board. The application works fine on the board with the CCS debugger. Now I am trying to flash it to NAND on the board and I am having NO luck. I used AISgen_d800k008 and flash writer provided with starter ware which is sfh_OMAP-L138.exe. I used the OMAPL138_LCDK_AISGen_Config.cfg in the AISgen. The nand flash 16bits and the some pll settings are automatically set by the .cfg.
The steps work fine. That is I can AISGen the app.out to produce app.bin. Then I can use sfh utility to connect to the lcdk via uart (with BOOTME) prompt and erase the flash and then write the image to flash. The steps go without a problem.
For the sfh I use the following steps.
sfh_OMAP-L138.exe -targettype C6748_LCDK -flashtype NAND -p COMx -erase
Flash bootable AIS image (ais_image.bin) to block 1 of the NAND:
sfh_OMAP-L138.exe -targettype C6748_LCDK -flashtype NAND -p COMx -flash_noubl ais_image.bin
However when I change the dip switches to boot from NAND flash and power cycle the board nothing happens. I am expecting to see a banner out put from the serial port. on my computer.
I then built the SerialEcho example in starter ware and ran it using CCS and debugger and works fine. Same story as above when I flashed it and tried to boot without the debugger attached. I have attached the linker map from the SerialEcho program. I am trying to run everything from L2 RAM. My final application will also run from L2 ram entirely.
Please let me know exact steps to follow from a known working tools. Where to download them from etc as several versions of the above tools seems to be floating around. I think there should be a utility integrated with CCS which will allow hapless engineers like me to easily flash target boards which will save a lot of development time.
Another question is can I boot from SD card on the LCDK? If possible can you point me to some information regarding this as well?
Thanks and best regards
Manjula
******************************************************************************
TMS320C6x Linker PC v7.4.15
******************************************************************************
>> Linked Fri Oct 30 01:27:16 2015
OUTPUT FILE NAME: <uart.out>
ENTRY POINT SYMBOL: "_c_int00" address: 11803400
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
DSPL2ROM 00700000 00100000 00000000 00100000 RWIX
DSPL2RAM 00800000 00040000 00000000 00040000 RWIX
DSPL1PRAM 00e00000 00008000 00000000 00008000 RWIX
DSPL1DRAM 00f00000 00008000 00000000 00008000 RWIX
SHDSPL2ROM 11700000 00100000 00000000 00100000 RWIX
SHDSPL2RAM 11800000 00040000 0000404c 0003bfb4 RWIX
SHDSPL1PRAM 11e00000 00008000 00000000 00008000 RWIX
SHDSPL1DRAM 11f00000 00008000 00000000 00008000 RWIX
EMIFACS0 40000000 20000000 00000000 20000000 RWIX
EMIFACS2 60000000 02000000 00000000 02000000 RWIX
EMIFACS3 62000000 02000000 00000000 02000000 RWIX
EMIFACS4 64000000 02000000 00000000 02000000 RWIX
EMIFACS5 66000000 02000000 00000000 02000000 RWIX
SHRAM 80000000 00020000 00000000 00020000 RWIX
DDR2 c0000000 20000000 00000000 20000000 RWIX
SEGMENT ALLOCATION MAP
run origin load origin length init length attrs members
---------- ----------- ---------- ----------- ----- -------
11800000 11800000 00003580 00003580 r-x
11800000 11800000 00003580 00003580 r-x .text
11803580 11803580 00000a40 00000000 rw-
11803580 11803580 00000800 00000000 rw- .stack
11803d80 11803d80 00000240 00000000 rw- .far
11803fc0 11803fc0 0000002c 0000002c rw-
11803fc0 11803fc0 00000024 00000024 rw- .fardata
11803fe4 11803fe4 00000008 00000008 rw- .neardata
11803ff0 11803ff0 00000060 00000060 r--
11803ff0 11803ff0 00000060 00000060 r-- .cinit
SECTION ALLOCATION MAP
output attributes/
section page origin length input sections
-------- ---- ---------- ---------- ----------------
.init_array
* 0 11800000 00000000 UNINITIALIZED
.text 0 11800000 00003580
11800000 00001aa0 interrupt.obj (.text:retain)
11801aa0 000005e0 interrupt.obj (.text)
11802080 00000580 uart.obj (.text)
11802600 00000200 uartEcho.obj (.text)
11802800 00000200 intvecs.obj (.text)
11802a00 00000180 rts6740_elf.lib : copy_decompress_rle.obj (.text:__TI_decompress_rle_core)
11802b80 00000180 uart_6748plat.obj (.text)
11802d00 00000140 psc.obj (.text)
11802e40 00000100 rts6740_elf.lib : autoinit.obj (.text:_auto_init_elf)
11802f40 00000100 : cpy_tbl.obj (.text:copy_in)
11803040 000000e0 : copy_zero_init.obj (.text:decompress:ZI:__TI_zero_init)
11803120 000000c0 : divu.obj (.text:__divu)
118031e0 000000c0 : exit.obj (.text:exit)
118032a0 000000c0 : tls.obj (.text:tls:init:__TI_tls_init)
11803360 000000a0 : memcpy64.obj (.text:memcpy)
11803400 00000080 : boot.obj (.text:_c_int00)
11803480 00000060 : cpp_init.obj (.text:__TI_cpp_init)
118034e0 00000040 : args_main.obj (.text:_args_main)
11803520 00000020 : exit.obj (.text:abort)
11803540 00000020 : copy_decompress_none.obj (.text:decompress:none:__TI_decompress_none)
11803560 00000020 : copy_decompress_rle.obj (.text:decompress:rle24:__TI_decompress_rle24)
.stack 0 11803580 00000800 UNINITIALIZED
11803580 00000008 rts6740_elf.lib : boot.obj (.stack)
11803588 000007f8 --HOLE--
.far 0 11803d80 00000240 UNINITIALIZED
11803d80 00000240 interrupt.obj (.far)
.fardata 0 11803fc0 00000024
11803fc0 00000018 uartEcho.obj (.fardata:txArray)
11803fd8 0000000c rts6740_elf.lib : exit.obj (.fardata)
.neardata
* 0 11803fe4 00000008
11803fe4 00000008 uartEcho.obj (.neardata)
.cinit 0 11803ff0 00000060
11803ff0 00000024 (.cinit..fardata.load) [load image, compression = rle]
11804014 0000000c (__TI_handler_table)
11804020 0000000a (.cinit..neardata.load) [load image, compression = rle]
1180402a 00000002 --HOLE-- [fill = 0]
1180402c 00000008 (.cinit..far.load) [load image, compression = zero_init]
11804034 00000004 --HOLE-- [fill = 0]
11804038 00000018 (__TI_cinit_table)
LINKER GENERATED COPY TABLES
__TI_cinit_table @ 11804038 records: 3, size/record: 8, table size: 24
.fardata: load addr=11803ff0, load size=00000024 bytes, run addr=11803fc0, run size=00000024 bytes, compression=rle
.neardata: load addr=11804020, load size=0000000a bytes, run addr=11803fe4, run size=00000008 bytes, compression=rle
.far: load addr=1180402c, load size=00000008 bytes, run addr=11803d80, run size=00000240 bytes, compression=zero_init
LINKER GENERATED HANDLER TABLE
__TI_handler_table @ 11804014 records: 3, size/record: 4, table size: 12
index: 0, handler: __TI_zero_init
index: 1, handler: __TI_decompress_rle24
index: 2, handler: __TI_decompress_none
GLOBAL SYMBOLS: SORTED ALPHABETICALLY BY Name
address name
-------- ----
11803520 C$$EXIT
11801ef8 ExcCombineAdd
11801f40 ExcCombineRemove
11801ed8 ExcGlobalEnable
11801aa0 IntDSPINTCInit
11801e50 IntDisable
11801e20 IntEnable
11801c18 IntEventClear
11801d54 IntEventCombineAdd
11801c50 IntEventCombineInit
11801df8 IntEventCombineRegister
11801da8 IntEventCombineRemove
11801b5c IntEventMap
11801be4 IntEventSet
11801eac IntGlobalDisable
11801e98 IntGlobalEnable
11801ec0 IntGlobalRestore
11801b10 IntRegister
11801e84 IntReset
11801b34 IntUnRegister
11802d00 PSCModuleControl
118024e4 UARTBreakCtl
118023d4 UARTCharGet
118023a8 UARTCharGetNonBlocking
11802410 UARTCharPut
11802368 UARTCharPutNonBlocking
11802318 UARTCharsAvail
11802114 UARTConfigGetExpClk
11802080 UARTConfigSetExpClk
118021ec UARTDMADisable
118021cc UARTDMAEnable
11802294 UARTDisable
11802278 UARTEnable
118022d4 UARTFIFODisable
118022c0 UARTFIFOEnable
118021a8 UARTFIFOLevelSet
11802490 UARTIntDisable
11802468 UARTIntEnable
118024b8 UARTIntStatus
11802570 UARTModemControlClear
118025a4 UARTModemControlGet
11802518 UARTModemControlSet
118025c4 UARTModemStatusGet
11802254 UARTParityModeGet
1180220c UARTParityModeSet
11802b80 UARTPinMuxSetup
11802348 UARTRxErrorGet
118022ec UARTSpaceAvail
11804038 __TI_CINIT_Base
11804050 __TI_CINIT_Limit
11804014 __TI_Handler_Table_Base
11804020 __TI_Handler_Table_Limit
UNDEFED __TI_INITARRAY_Base
UNDEFED __TI_INITARRAY_Limit
11803d80 __TI_STACK_END
00000800 __TI_STACK_SIZE
11803fe4 __TI_STATIC_BASE
UNDEFED __TI_TLS_INIT_Base
UNDEFED __TI_TLS_INIT_Limit
00000001 __TI_args_main
11803480 __TI_cpp_init
11803540 __TI_decompress_none
11803560 __TI_decompress_rle24
11803fe0 __TI_enable_exit_profile_output
ffffffff __TI_pprof_out_hndl
ffffffff __TI_prof_data_size
ffffffff __TI_prof_data_start
118032a0 __TI_tls_init
11803040 __TI_zero_init
ffffffff __binit__
11803120 __c6xabi_divu
ffffffff __c_args__
11803120 __divu
118034e0 _args_main
11802e40 _auto_init_elf
11800ff8 _c674x_mask_int10_isr
118011c0 _c674x_mask_int11_isr
11801384 _c674x_mask_int12_isr
11801548 _c674x_mask_int13_isr
11801710 _c674x_mask_int14_isr
118018d8 _c674x_mask_int15_isr
11800550 _c674x_mask_int4_isr
11800718 _c674x_mask_int5_isr
118008e0 _c674x_mask_int6_isr
11800aa4 _c674x_mask_int7_isr
11800c68 _c674x_mask_int8_isr
11800e30 _c674x_mask_int9_isr
11800000 _c674x_nmi_isr
118001c4 _c674x_rsvd_int2_isr
11800388 _c674x_rsvd_int3_isr
11803400 _c_int00
11803fd8 _cleanup_ptr
11803fdc _dtors_ptr
11802800 _intcVectorTable
11803580 _stack
11803520 abort
ffffffff binit
11802f40 copy_in
118031e0 exit
11802600 main
11803360 memcpy
11803fc0 txArray
GLOBAL SYMBOLS: SORTED BY Symbol Address
address name
-------- ----
00000001 __TI_args_main
00000800 __TI_STACK_SIZE
11800000 _c674x_nmi_isr
118001c4 _c674x_rsvd_int2_isr
11800388 _c674x_rsvd_int3_isr
11800550 _c674x_mask_int4_isr
11800718 _c674x_mask_int5_isr
118008e0 _c674x_mask_int6_isr
11800aa4 _c674x_mask_int7_isr
11800c68 _c674x_mask_int8_isr
11800e30 _c674x_mask_int9_isr
11800ff8 _c674x_mask_int10_isr
118011c0 _c674x_mask_int11_isr
11801384 _c674x_mask_int12_isr
11801548 _c674x_mask_int13_isr
11801710 _c674x_mask_int14_isr
118018d8 _c674x_mask_int15_isr
11801aa0 IntDSPINTCInit
11801b10 IntRegister
11801b34 IntUnRegister
11801b5c IntEventMap
11801be4 IntEventSet
11801c18 IntEventClear
11801c50 IntEventCombineInit
11801d54 IntEventCombineAdd
11801da8 IntEventCombineRemove
11801df8 IntEventCombineRegister
11801e20 IntEnable
11801e50 IntDisable
11801e84 IntReset
11801e98 IntGlobalEnable
11801eac IntGlobalDisable
11801ec0 IntGlobalRestore
11801ed8 ExcGlobalEnable
11801ef8 ExcCombineAdd
11801f40 ExcCombineRemove
11802080 UARTConfigSetExpClk
11802114 UARTConfigGetExpClk
118021a8 UARTFIFOLevelSet
118021cc UARTDMAEnable
118021ec UARTDMADisable
1180220c UARTParityModeSet
11802254 UARTParityModeGet
11802278 UARTEnable
11802294 UARTDisable
118022c0 UARTFIFOEnable
118022d4 UARTFIFODisable
118022ec UARTSpaceAvail
11802318 UARTCharsAvail
11802348 UARTRxErrorGet
11802368 UARTCharPutNonBlocking
118023a8 UARTCharGetNonBlocking
118023d4 UARTCharGet
11802410 UARTCharPut
11802468 UARTIntEnable
11802490 UARTIntDisable
118024b8 UARTIntStatus
118024e4 UARTBreakCtl
11802518 UARTModemControlSet
11802570 UARTModemControlClear
118025a4 UARTModemControlGet
118025c4 UARTModemStatusGet
11802600 main
11802800 _intcVectorTable
11802b80 UARTPinMuxSetup
11802d00 PSCModuleControl
11802e40 _auto_init_elf
11802f40 copy_in
11803040 __TI_zero_init
11803120 __c6xabi_divu
11803120 __divu
118031e0 exit
118032a0 __TI_tls_init
11803360 memcpy
11803400 _c_int00
11803480 __TI_cpp_init
118034e0 _args_main
11803520 C$$EXIT
11803520 abort
11803540 __TI_decompress_none
11803560 __TI_decompress_rle24
11803580 _stack
11803d80 __TI_STACK_END
11803fc0 txArray
11803fd8 _cleanup_ptr
11803fdc _dtors_ptr
11803fe0 __TI_enable_exit_profile_output
11803fe4 __TI_STATIC_BASE
11804014 __TI_Handler_Table_Base
11804020 __TI_Handler_Table_Limit
11804038 __TI_CINIT_Base
11804050 __TI_CINIT_Limit
ffffffff __TI_pprof_out_hndl
ffffffff __TI_prof_data_size
ffffffff __TI_prof_data_start
ffffffff __binit__
ffffffff __c_args__
ffffffff binit
UNDEFED __TI_INITARRAY_Base
UNDEFED __TI_INITARRAY_Limit
UNDEFED __TI_TLS_INIT_Base
UNDEFED __TI_TLS_INIT_Limit
[102 symbols]