Good morning,
We have following desire:
We want to restart our Sitara with Sysbios after an abnormal/normal termination.
Actually we are using two functions which are connected to the SysCallback functions
SysCallback.abortFxn = "&callback_WebconsoleAbortFxn";
SysCallback.exitFxn = "&callback_WebconsoleExitFxn";
These functions are called on an abort or exit.
Is there a way to restart the complete system via software?
Thanks in advance.
Kind regards,
Raul
Code Composer Version: 6.1.0.00104
SYS/BIOS 6.41.00.26
XDCTools 3.31.00.24 core
NDK 2.24.01.18