-
Dear everyone,The following information was showed in my console. I wonder if it is a proplem of Gel or cmd file?CCS version:6.1.1; MCSDK: 3.01.04.07; The default tcievmk2l.gel is chosen.C66xx_0: GEL Output: DDR begin
C66xx_0: GEL Output: XMC setup complete.
C66xx_0: GEL Output: DDR3 PLL Setup ...
C66xx_0: GEL Output: DDR3 PLL Setup complete, DDR3A clock now running at 533MHz.
C66xx_0: GEL Output: DDR3A initialization complete
C66xx_0: GEL Output: DDR done
C66xx_0: Trouble Reading Memory Block at 0x8000 on Page 0 of Length 0x4: (Error -1190 @ 0x8000) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.14.5)
C66xx_0: File Loader: Verification failed: Target failed to read 0x00008000
Thanks for your advice.