Hello,
While using the can driver i get the following error:
swapper page allocation failure order 0 mode 0x20
googling a bit says increase the sizes but doesnt help.
Thanks,
Mike
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
mike A said:I have custom DM8148 board
Can you test on DM8148 TI EVM (1GB DDR3)?
mike A said:I can get can frames when using candump, but after sometime (10mins) I get this allocation error issue.
You need to provide enough space for kernel on RAM. Driver seems not be able to allocate memory from kernel. You might need to tune your bootargs and/or check for memory leak. See if the below pointers will help:



BR
Pavel