HI ,
I am interfacing PMIC(TPS65910A) interfacing with AM3352 Processor. As per AM3352 power sequence, PMIC pins value to be BOOT1=1 and BOOT0 =0 which is EEPROM boot mode, recommneded in TPS65910x user guide for AM335X . While in PMIC datasheet on page no 38, BOOT1=0, BOOT0= 1. is given as EEPROM mode. IN PMIC datasheet BOOT1=1, BOOT0= 0 is not given so i want to check if it is typing mistake in PMIC datasheet. Whihc power sequence i should refer in PMIC datasheet for AM335X mpu power sequence.
I want to confirm that what should be the actual boot mode pin value(BOOT1=?, BOOT0= ?) for Am3352 MPU for TPS65910A.
Regards
Manoj A