This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to make cpsw_emac1 as default and only ETH0 device on am335x-evmsk base on ti-processor-sdk-linux-am335x-evm-01.00.00.03 ?

Other Parts Discussed in Thread: TFP410, TPS65910

Hi,

I work on  am335x-evmsk base on sdk-8 [ ti-processor-sdk-linux-am335x-evm-01.00.00.03 ] and I try  to make  cpsw_emac1  as default and only ETH0 device ,

but I don't success.

Attach is how I defined it in DTS file and boot log:

cpsw_default: cpsw_default {
  pinctrl-single,pins = <
   0x78 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (U18) gpmc_be1n.gmii2_col */
   0x70 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (T17) gpmc_wait0.gmii2_crs */
   0x74 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (U17) gpmc_wpn.gmii2_rxer */
   0x40 ( PIN_OUTPUT_PULLDOWN | MUX_MODE1 ) /* (R13) gpmc_a0.gmii2_txen */
   0x44 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (V14) gpmc_a1.gmii2_rxdv */
   0x58 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (U15) gpmc_a6.gmii2_txclk */
   0x5c ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (T15) gpmc_a7.gmii2_rxclk */
   0x54 ( PIN_OUTPUT_PULLDOWN | MUX_MODE1 ) /* (V15) gpmc_a5.gmii2_txd0 */
   0x50 ( PIN_OUTPUT_PULLDOWN | MUX_MODE1 ) /* (R14) gpmc_a4.gmii2_txd1 */
   0x4c ( PIN_OUTPUT_PULLDOWN | MUX_MODE1 ) /* (T14) gpmc_a3.gmii2_txd2 */
   0x48 ( PIN_OUTPUT_PULLDOWN | MUX_MODE1 ) /* (U14) gpmc_a2.gmii2_txd3 */
   0x6c ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (V17) gpmc_a11.gmii2_rxd0 */
   0x68 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (T16) gpmc_a10.gmii2_rxd1 */
   0x64 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (U16) gpmc_a9.gmii2_rxd2 */
   0x60 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (V16) gpmc_a8.gmii2_rxd3 */
  >;
 };

 /* Optional sleep pin settings. Must manually enter values in the below skeleton. */
 cpsw_sleep: cpsw_sleep {
  pinctrl-single,pins = <
   0x78 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (U18) gpmc_be1n.gmii2_col */
   0x70 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (T17) gpmc_wait0.gmii2_crs */
   0x74 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (U17) gpmc_wpn.gmii2_rxer */
   0x40 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (R13) gpmc_a0.gmii2_txen */
   0x44 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (V14) gpmc_a1.gmii2_rxdv */
   0x58 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (U15) gpmc_a6.gmii2_txclk */
   0x5c (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (T15) gpmc_a7.gmii2_rxclk */
   0x54 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (V15) gpmc_a5.gmii2_txd0 */
   0x50 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (R14) gpmc_a4.gmii2_txd1 */
   0x4c (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (T14) gpmc_a3.gmii2_txd2 */
   0x48 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (U14) gpmc_a2.gmii2_txd3 */
   0x6c (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (V17) gpmc_a11.gmii2_rxd0 */
   0x68 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (T16) gpmc_a10.gmii2_rxd1 */
   0x64 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (U16) gpmc_a9.gmii2_rxd2 */
   0x60 (PIN_INPUT_PULLDOWN | MUX_MODE7 ) /* (V16) gpmc_a8.gmii2_rxd3 */
  >;
 };
 

 davinci_mdio_default: davinci_mdio_default {
  pinctrl-single,pins = <
   /* MDIO */
   0x148 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0) /* mdio_data.mdio_data */
   0x14c (PIN_OUTPUT_PULLUP | MUX_MODE0)   /* mdio_clk.mdio_clk */
  >;
 };

 davinci_mdio_sleep: davinci_mdio_sleep {
  pinctrl-single,pins = <
   /* MDIO reset value */
   0x148 (PIN_INPUT_PULLDOWN | MUX_MODE7)
   0x14c (PIN_INPUT_PULLDOWN | MUX_MODE7)
  >;
 };

&mac {
 pinctrl-names = "default", "sleep";
 pinctrl-0 = <&cpsw_default>;
 pinctrl-1 = <&cpsw_sleep>;
 dual_emac = <1>;
       
};

&davinci_mdio {
 pinctrl-names = "default", "sleep";
 pinctrl-0 = <&davinci_mdio_default>;
 pinctrl-1 = <&davinci_mdio_sleep>;
};

&cpsw_emac0 {
 phy_id = <&davinci_mdio>, <0>;
 phy-mode = "rgmii-txid";
 dual_emac_res_vlan = <1>;
};

&cpsw_emac1 {
 phy_id = <&davinci_mdio>, <1>;
 phy-mode = "rgmii-txid";
 dual_emac_res_vlan = <2>;
};

boot log:

U-Boot SPL 2014.07-00001-g4a8e5b8-dirty (Sep 30 2015 - 16:37:01)
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img


U-Boot 2014.07-00001-g4a8e5b8-dirty (Sep 30 2015 - 16:37:01)

I2C:   ready
DRAM:  256 MiB
NAND:  0 MiB
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env

** Unable to read "uboot.env" from mmc0:1 **
Using default environment

Net:   <ethaddr> not set. Validating first E-fuse MAC
Phy not found
cpsw, usb_ether
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
** Unable to read file uEnv.txt **
4342632 bytes read in 308 ms (13.4 MiB/s)
37426 bytes read in 18 ms (2 MiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x424368 ]
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 8e713000, end 8e71f231 ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 3.14.43-g875c69b (root@ubuntu) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #15 Sun Nov 1 12:06:08 IST 2015
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine model: TI AM335x EVM-SK
[    0.000000] cma: CMA: reserved 24 MiB at 8c800000
[    0.000000] Memory policy: Data cache writeback
[    0.000000] CPU: All CPU(s) started in SVC mode.
[    0.000000] AM335X ES2.1 (neon )
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 64768
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait
[    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[    0.000000] Memory: 225260K/261120K available (5851K kernel code, 303K rwdata, 2148K rodata, 260K init, 232K bss, 35860K reserved, 0K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc07d80c4   (8001 kB)
[    0.000000]       .init : 0xc07d9000 - 0xc081a2a4   ( 261 kB)
[    0.000000]       .data : 0xc081c000 - 0xc0867e20   ( 304 kB)
[    0.000000]        .bss : 0xc0867e20 - 0xc08a1eb8   ( 233 kB)
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] Total of 128 interrupts on 1 active controller
[    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[    0.000017] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956969942ns
[    0.000042] OMAP clocksource: timer1 at 24000000 Hz
[    0.000371] Console: colour dummy device 80x30
[    0.000400] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[    0.000408] This ensures that you still see kernel messages. Please
[    0.000415] update your kernel commandline.
[    0.000443] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032)
[    0.059170] pid_max: default: 32768 minimum: 301
[    0.059300] Security Framework initialized
[    0.059371] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.059386] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.069168] CPU: Testing write buffer coherency: ok
[    0.069683] Setting up static identity map for 0x805bce60 - 0x805bceb8
[    0.070839] devtmpfs: initialized
[    0.073076] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    0.082672] omap_hwmod: tptc0 using broken dt data from edma
[    0.082778] omap_hwmod: tptc1 using broken dt data from edma
[    0.082872] omap_hwmod: tptc2 using broken dt data from edma
[    0.087448] omap_hwmod: debugss: _wait_target_disable failed
[    0.144402] pinctrl core: initialized pinctrl subsystem
[    0.145637] regulator-dummy: no parameters
[    0.148324] NET: Registered protocol family 16
[    0.150894] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.154082] cpuidle: using governor ladder
[    0.154104] cpuidle: using governor menu
[    0.162384] syscon 44e10000.control_module: regmap [mem 0x44e10000-0x44e107fb] registered
[    0.164229] platform 49000000.edma: alias fck already exists
[    0.164260] platform 49000000.edma: alias fck already exists
[    0.164279] platform 49000000.edma: alias fck already exists
[    0.165705] OMAP GPIO hardware version 0.1
[    0.184917] No ATAGs?
[    0.184943] hw-breakpoint: debug architecture 0x4 unsupported.
[    0.219096] bio: create slab <bio-0> at 0
[    0.239912] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[    0.241179] vbat: 5000 mV
[    0.241669] lis3_reg: no parameters
[    0.242285] wlan-en-regulator: 1800 mV
[    0.242873] vtt: 1500 mV
[    0.246960] vgaarb: loaded
[    0.247633] i2c-core: driver [palmas] using legacy suspend method
[    0.247647] i2c-core: driver [palmas] using legacy resume method
[    0.248547] SCSI subsystem initialized
[    0.250540] usbcore: registered new interface driver usbfs
[    0.250796] usbcore: registered new interface driver hub
[    0.251055] usbcore: registered new device driver usb
[    0.252283] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c0_pins, deferring probe
[    0.252320] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral
[    0.252831] pps_core: LinuxPPS API ver. 1 registered
[    0.252845] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.253011] PTP clock support registered
[    0.255486] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[    0.256607] Advanced Linux Sound Architecture Driver Initialized.
[    0.258608] Switched to clocksource timer1
[    0.283735] NET: Registered protocol family 2
[    0.284841] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[    0.284884] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[    0.284921] TCP: Hash tables configured (established 2048 bind 2048)
[    0.284997] TCP: reno registered
[    0.285013] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.285037] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.285250] NET: Registered protocol family 1
[    0.285690] RPC: Registered named UNIX socket transport module.
[    0.285705] RPC: Registered udp transport module.
[    0.285714] RPC: Registered tcp transport module.
[    0.285722] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.287013] hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available
[    0.290598] futex hash table entries: 256 (order: -1, 3072 bytes)
[    0.511809] VFS: Disk quotas dquot_6.5.2
[    0.511889] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.512524] NFS: Registering the id_resolver key type
[    0.512611] Key type id_resolver registered
[    0.512622] Key type id_legacy registered
[    0.512670] jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
[    0.512884] msgmni has been set to 487
[    0.514724] NET: Registered protocol family 38
[    0.514775] io scheduler noop registered
[    0.514787] io scheduler deadline registered
[    0.514822] io scheduler cfq registered (default)
[    0.516940] pinctrl-single 44e10800.pinmux: bad data for mux pinmux_clkout2_pin
[    0.516965] pinctrl-single 44e10800.pinmux: no pins entries for pinmux_clkout2_pin
[    0.517054] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[    0.521959] backlight supply power not found, using dummy regulator
[    0.526722] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[    0.533463] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) is a 8250
[    1.185962] console [ttyS0] enabled
[    1.190888] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 89, base_baud = 3000000) is a 8250
[    1.201980] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[    1.209204] [drm] Initialized drm 1.1.0 20060810
[    1.227648] brd: module loaded
[    1.237981] loop: module loaded
[    1.241606] (stk) :sysfs entries created
[    1.245602] (stk) : debugfs entries created
[    1.250007] (hci_tty): inside hci_tty_init
[    1.254895] (hci_tty): allocated 250, 0
[    1.263980] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.275442] usbcore: registered new interface driver asix
[    1.281187] usbcore: registered new interface driver ax88179_178a
[    1.287542] usbcore: registered new interface driver cdc_ether
[    1.293638] usbcore: registered new interface driver smsc95xx
[    1.299647] usbcore: registered new interface driver net1080
[    1.305559] usbcore: registered new interface driver cdc_subset
[    1.311696] usbcore: registered new interface driver zaurus
[    1.317605] usbcore: registered new interface driver cdc_ncm
[    1.323969] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.330565] ehci-pci: EHCI PCI platform driver
[    1.335277] ehci-omap: OMAP-EHCI Host Controller driver
[    1.341207] usbcore: registered new interface driver cdc_acm
[    1.346899] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[    1.355198] usbcore: registered new interface driver cdc_wdm
[    1.361156] usbcore: registered new interface driver usb-storage
[    1.368585] mousedev: PS/2 mouse device common for all mice
[    1.376391] input: ti-tsc as /devices/ocp/44e0d000.tscadc/TI-am335x-tsc/input/input0
[    1.386039] i2c-core: driver [rtc-ds1307] using legacy suspend method
[    1.392566] i2c-core: driver [rtc-ds1307] using legacy resume method
[    1.399897] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[    1.407029] 44e3e000.rtc: already running
[    1.412153] i2c /dev entries driver
[    1.415866] Driver for 1-wire Dallas network protocol.
[    1.424085] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    1.433514] omap_hsmmc 48060000.mmc: unable to get vmmc regulator -517
[    1.440442] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral
[    1.563943] omap_hsmmc 481d8000.mmc: card claims to support voltages below defined range
[    1.573913] ledtrig-cpu: registered to indicate activity on CPUs
[    1.580480] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[    1.587975] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[    1.595901] usbcore: registered new interface driver usbhid
[    1.601550] usbhid: USB HID core driver
[    1.605784] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[    1.617348] oprofile: using arm/armv7
[    1.621563] TCP: cubic registered
[    1.624910] Initializing XFRM netlink socket
[    1.629282] NET: Registered protocol family 17
[    1.633796] NET: Registered protocol family 15
[    1.638402] Key type dns_resolver registered
[    1.643852] mmc0: queuing unknown CIS tuple 0x91 (3 bytes)
[    1.649954] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
[    1.658753] cpu cpu0: cpu0 clock notifier not ready, retry
[    1.664467] platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
[    1.672730] PM: bootloader does not support rtc-only!
[    1.677823] ThumbEE CPU extension supported.
[    1.682393] Registering SWP/SWPB emulation handler
[    1.688977] mmc0: new high speed SDIO card at address 0001
[    1.695478] lis3_reg: disabling
[    1.698771] vbat: disabling
[    1.701583] regulator-dummy: disabling
[    1.708171] Error: Driver 'tfp410' is already registered, aborting...
[    1.717720] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    1.724439] [drm] No driver support for vblank timestamp query.
[    1.781618] Console: switching to colour frame buffer device 60x34
[    1.790674] tilcdc 4830e000.lcdc: fb0:  frame buffer device
[    1.796285] tilcdc 4830e000.lcdc: registered panic notifier
[    1.801972] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[    1.810792] tps65910 0-002d: No interrupt support, no core IRQ
[    1.821545] vrtc: 1800 mV
[    1.824598] vrtc: supplied by vbat
[    1.829960] vio: at 1500 mV
[    1.832977] vio: supplied by vbat
[    1.838349] vdd_mpu: 912 <--> 1375 mV at 1137 mV
[    1.843204] vdd_mpu: supplied by vbat
[    1.848954] vdd_core: 912 <--> 1150 mV at 1137 mV
[    1.853883] vdd_core: supplied by vbat
[    1.859186] vdd3: 5000 mV
[    1.863437] vdig1: at 1800 mV
[    1.866595] vdig1: supplied by vbat
[    1.871707] vdig2: at 1800 mV
[    1.874861] vdig2: supplied by vbat
[    1.879942] vpll: at 1800 mV
[    1.883005] vpll: supplied by vbat
[    1.887979] vdac: at 1800 mV
[    1.891082] vdac: supplied by vbat
[    1.896070] vaux1: at 1800 mV
[    1.899246] vaux1: supplied by vbat
[    1.904306] vaux2: at 3300 mV
[    1.907474] vaux2: supplied by vbat
[    1.912573] vaux33: at 3300 mV
[    1.915817] vaux33: supplied by vbat
[    1.920949] vmmc: 1800 <--> 3300 mV at 3300 mV
[    1.925589] vmmc: supplied by vbat
[    1.931272] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[    1.979377]  remoteproc0: wkup_m3 is available
[    1.983860]  remoteproc0: Note: remoteproc is still under development and considered experimental.
[    1.992918]  remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[    2.003570]  remoteproc0: Direct firmware load failed with error -2
[    2.009957]  remoteproc0: Falling back to user helper
[    2.078658] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[    2.084813] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[    2.091987] libphy: 4a101000.mdio: probed
[    2.096038] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[    2.106313] cpsw 4a100000.ethernet: Detected MACID = 68:c9:0b:30:2d:54
[    2.114576] cpsw 4a100000.ethernet: cpsw: Detected MACID = 68:c9:0b:30:2d:56
[    2.124707] input: gpio_buttons@0 as /devices/gpio_buttons@0/input/input1
[    2.132578] omap_rtc 44e3e000.rtc: setting system clock to 2015-10-29 14:29:06 UTC (1446128946)
[    2.145148] ALSA device list:
[    2.148152]   No soundcards found.
[    2.151745] mmc1: host does not support reading read-only switch. assuming write-enable.
[    2.160533] Waiting for root device /dev/mmcblk0p2...
[    2.169109] mmc1: new high speed SDHC card at address aaaa
[    2.175537] mmcblk0: mmc1:aaaa SU08G 7.40 GiB
[    2.182126]  mmcblk0: p1 p2
[    2.273139] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem
[    2.280560] EXT4-fs (mmcblk0p2): write access will be enabled during recovery
[    2.331105] EXT4-fs (mmcblk0p2): recovery complete
[    2.345118] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    2.353483] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
[    2.364479] devtmpfs: mounted
[    2.368547] Freeing unused kernel memory: 260K (c07d9000 - c081a000)
INIT: version 2.88 booting
Starting udev
[    3.201791] udevd[876]: starting version 182
[    3.474838] Bluetooth: Core ver 2.18
[    3.478558] NET: Registered protocol family 31
[    3.483137] Bluetooth: HCI device and connection manager initialized
[    3.708595]  remoteproc0: powering up wkup_m3
[    3.738802] Bluetooth: HCI socket layer initialized
[    3.754889]  remoteproc0: Booting fw image am335x-pm-firmware.elf, size 154412
[    3.812113] lis3lv02d: unknown sensor type 0x87
[    3.816817] lis3lv02d_i2c: probe of 0-0018 failed with error -22
[    3.834051] Bluetooth: L2CAP socket layer initialized
[    3.870900] PM: CM3 Firmware Version = 0x190
[    3.898992] Bluetooth: SCO socket layer initialized
[    3.918761]  remoteproc0: remote processor wkup_m3 is now up
[    3.968442] (stc):  chnl_id list empty :4
[    3.972496] (stk) : st_kim_start(stk) :ldisc_install = 1
[    4.116378] cryptodev: driver 1.6 loaded.
[    4.146409] 47401300.usb-phy supply vcc not found, using dummy regulator
[    4.280635] 47401b00.usb-phy supply vcc not found, using dummy regulator
[    4.566068] EXT4-fs (mmcblk0p2): re-mounted. Opts: data=ordered
[    4.616055] Loading modules backported from Linux version R8.5-2-gad69b45
[    4.623005] Backport generated by backports.git R8.4-0-g0d46f43
Starting Bootlog daemon: [    5.088763] (stk) :ldisc installation timeout
[    5.093005] (stk) :ldisc_install = 0bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
[    5.383926] random: dd urandom read with 106 bits of entropy available
[    5.519516] davinci_evm sound: tlv320aic3x-hifi <-> 4803c000.mcasp mapping ok
[    6.088741] (stk) : timed out waiting for ldisc to be un-installed
[    6.201573] (stk) :ldisc_install = 1
udevadm settle - timeout of 3 seconds reached, the event queue contains:
  /sys/devices/ocp/48060000.mmc/mmc_host/mmc1/mmc1:aaaa/block/mmcblk0/mmcblk0p1 (862)
  /sys/devices/ocp/48060000.mmc/mmc_host/mmc1/mmc1:aaaa/block/mmcblk0/mmcblk0p2 (863)
  /sys/devices/virtual/block/loop0 (1012)
  /sys/devices/virtual/block/loop1 (1013)
  /sys/devices/virtual/block/loop2 (1014)
  /sys/devices/virtual/block/loop3 (1015)
  /sys/devices/virtual/block/loop4 (1016)
  /sys/devices/virtual/block/loop5 (1017)
  /sys/devices/virtual/block/loop6 (1018)
  /sys/devices/virtual/block/loop7 (1019)
  /sys/devices/virtual/block/ram0 (1020)
  /sys/devices/virtual/block/ram1 (1021)
  /sys/devices/virtual/block/ram10 (1022)
  /sys/devices/virtual/block/ram11 (1023)
  /sys/devices/virtual/block/ram12 (1024)
  /sys/devices/virtual/block/ram13 (1025)
  /sys/devices/virtual/block/ram14 (1026)
  /sys/devices/virtual/block/ram15 (1027)
  /sys/devices/virtual/block/ram2 (1028)
  /sys/devices/virtual/block/ram3 (1029)
  /sys/devices/virtual/block/ram4 (1030)
  /sys/devices/virtual/block/ram5 (1031)
  /sys/devices/virtual/block/ram6 (1032)
  /sys/devices/virtual/block/ram7 (1033)
  /sys/devices/virtual/block/ram8 (1034)
  /sys/devices/virtual/block/ram9 (1035)
  /sys/devices/virtual/net/lo (1042)
  /sys/devices/virtual/bluetooth/hci0/rfkill0 (1057)
[    7.048874] random: nonblocking pool is initialized
[    7.198737] (stk) :ldisc installation timeout
[    7.202974] (stk) :ldisc_install = 0[    7.322639] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[    7.573325] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 1
[    7.749499] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    7.756369] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    7.763673] usb usb1: Product: MUSB HDRC host driver
[    7.768681] usb usb1: Manufacturer: Linux 3.14.43-g875c69b musb-hcd
[    7.774983] usb usb1: SerialNumber: musb-hdrc.1.auto
[    7.988058] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[    8.016521] hub 1-0:1.0: USB hub found
[    8.049124] hub 1-0:1.0: 1 port detected
[    8.077473] cfg80211: Calling CRDA to update world regulatory domain
[    8.097855] musb-hdrc musb-hdrc.2.auto: MUSB HDRC host driver
[    8.198752] (stk) : timed out waiting for ldisc to be un-installed
[    8.311606] (stk) :ldisc_install = 1[    8.325005] musb-hdrc musb-hdrc.2.auto: new USB bus registered, assigned bus number 2
[    8.391735] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[    8.398686] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    8.405950] usb usb2: Product: MUSB HDRC host driver
[    8.410961] usb usb2: Manufacturer: Linux 3.14.43-g875c69b musb-hcd
[    8.417265] usb usb2: SerialNumber: musb-hdrc.2.auto
[    8.492723] hub 2-0:1.0: USB hub found
[    8.536648] hub 2-0:1.0: 1 port detected
[    8.553490] wl18xx_driver wl18xx.0.auto: Direct firmware load failed with error -2
[    8.561197] wl18xx_driver wl18xx.0.auto: Falling back to user helper
[    8.573109] cfg80211: World regulatory domain updated:
[    8.578305] cfg80211:  DFS Master region: unset
[    8.582798] cfg80211:   (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
[    8.592627] cfg80211:   (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm), (N/A)
[    8.601033] cfg80211:   (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm), (N/A)
[    8.609458] cfg80211:   (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm), (N/A)
[    8.617850] cfg80211:   (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm), (N/A)
[    8.626259] cfg80211:   (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm), (N/A)
ALSA: Restoring mixer settings...
[    9.179663] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[    9.224314] wlcore: loaded
[    9.227140] wlcore: driver version: ol_r8.a9.14
[    9.231762] wlcore: compilation time: Mon Jul  6 16:06:06 2015
[    9.308784] (stk) :ldisc installation timeout
INIT: Entering runlevel: 5c_install = 0
Configuring network interfaces... [    9.744960] net eth0: initializing cpsw version 1.12 (0)
udhcpc (v1.22.1) started
Sending discover...
[   10.308672] (stk) : timed out waiting for ldisc to be un-installed
[   10.421494] (stk) :ldisc_install = 1(stk) :ldisc installation timeout
[   11.421594] (stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
[   12.530304] (stk) :ldisc_install = 1[   12.909271] libphy: 4a101000.mdio:00 - Link is Up - 100/Full
Sending discover...
[   13.528709] (stk) :ldisc installation timeout
[   13.532954] (stk) :ldisc_install = 0(stk) : timed out waiting for ldisc to be un-installed
[   14.640329] (stk) :ldisc_install = 1(stk) :ldisc installation timeout
[   15.641594] (stk) :ldisc_install = 0Sending discover...
(stk) : timed out waiting for ldisc to be un-installed
[   16.645453] Bluetooth: st_register failed -22
No lease, forking to background
done.
Starting system message bus: dbus.
UIM SYSFS Node Found at /sys/./devices/kim/install
Starting uim-sysfs daemon.
uim:@ main
uim:install = /sys/./devices/kim/install
uim:dev_name = /sys/./devices/kim/dev_name
uim:baud_rate = /sys/./devices/kim/baud_rate
uim:flow_cntrl = /sys/./devices/kim/flow_cntrl
uim:begin polling...
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting rpcbind daemon...rpcbind: cannot create socket for udp6
rpcbind: cannot create socket for tcp6
done.
creating NFS state directory: done
starting statd: done
Starting syslogd/klogd: done
Starting thttpd.
Starting PVR
insmod: ERROR: missing filename.
Could not find pvrsrvkm driver
Starting Lighttpd Web Server: lighttpd.
2015-10-29 14:29:24: (/home/gtbldadm/ti/oe-layersetup/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa8t2hf-vfp-neon-linux-gnueabi/lighttpd/1.4.33-r1/lighttpd-1.4.33/src/log.c.166) server started
no upgradeStarting PureCom ApplicationEnabling thermal zones...
/etc/rc5.d/S98thermal-zone-init: line 7: /sys/class/thermal/thermal_zone*/mode: No such file or directory
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
        autoconf
        binutils
        cpp-symlinks
        cpp
        g++-symlinks
        g++
        gcc-symlinks
        gcc
        gdbserver
        gstreamer1.0-libav
        libgmp10
        libmpc3
        libmpfr4
        make

If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution.  This can be done using
the opkg remove command.  i.e.:
    opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
      will be notified of the dependent packages.  You should
      use the --force-removal-of-dependent-packages option to
      also remove the dependent packages as well
***************************************************************
***************************************************************
Stopping Bootlog daemon: bootlogd.
umount: can't forcibly umount /mnt/.psplash: Invalid argument

 _____                    _____           _         _
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|

Arago Project http://arago-project.org am335x-evm /dev/ttyO0

Arago 2015.05 am335x-evm /dev/ttyO0

am335x-evm login: root
root@am335x-evm:~# ifconfig
eth0      Link encap:Ethernet  HWaddr 68:C9:0B:30:2D:54
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:2 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:684 (684.0 B)
          Interrupt:56

lo        Link encap:Local Loopback
          inet addr:127.0.0.1  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:10 errors:0 dropped:0 overruns:0 frame:0
          TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:700 (700.0 B)  TX bytes:700 (700.0 B)

root@am335x-evm:~#

Thanks Oded.

  • Hi,

    I will ask the Ethernet experts to comment if/how this is possible. Feedback will be posted directly here when available.
  • Hi Biser,

    To be more precise, I need that ethernet interface [ eth0 or eth1] will work only from P2 [ the port of eth1].
    How can I doit?

    Thanks Oded.
  • Hi Biser,

    To be more precise, I need that ethernet interface [ eth0 or eth1] will work only from P2 [ the port of eth1].
    Because currently I receive this when I boot:

    am335x-evm login: root
    root@am335x-evm:~# ifconfig
    eth0 Link encap:Ethernet HWaddr 68:C9:0B:30:2D:54
    UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:1 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:342 (342.0 B)
    Interrupt:56

    lo Link encap:Local Loopback
    inet addr:127.0.0.1 Mask:255.0.0.0
    UP LOOPBACK RUNNING MTU:65536 Metric:1
    RX packets:10 errors:0 dropped:0 overruns:0 frame:0
    TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:0
    RX bytes:700 (700.0 B) TX bytes:700 (700.0 B)

    root@am335x-evm:~# ifdown eth0
    root@am335x-evm:~# ifconfig
    lo Link encap:Local Loopback
    inet addr:127.0.0.1 Mask:255.0.0.0
    UP LOOPBACK RUNNING MTU:65536 Metric:1
    RX packets:10 errors:0 dropped:0 overruns:0 frame:0
    TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:0
    RX bytes:700 (700.0 B) TX bytes:700 (700.0 B)

    root@am335x-evm:~# ifup eth0
    [ 50.467132] net eth0: initializing cpsw version 1.12 (0)
    udhcpc (v1.22.1) started
    Sending discover...
    [ 53.629379] libphy: 4a101000.mdio:00 - Link is Up - 100/Full
    Sending discover...
    Sending discover...
    No lease, forking to background
    root@am335x-evm:~# ifdown eth0
    root@am335x-evm:~# ifup eth1
    [ 89.222002] net eth1: initializing cpsw version 1.12 (0)
    [ 89.230941] libphy: PHY 4a101000.mdio:01 not found
    udhcpc (v1.22.1) started
    Sending discover...
    Sending discover...
    Sending discover...
    No lease, forking to background
    root@am335x-evm:~#

    As you can see, after boot , eth0 don't have an ip ddress and eth1 receive " libphy: PHY 4a101000.mdio:01 not found
    " message after ifup eth1 operation.

    What the problems?


    Thanks Oded
  • Hi Oded,

    Is this the AM335X Starter Kit you are talking about? If this is correct you should note that the two Ethernet PHYs share a common crystal, that's physically connected to the eth0 PHY. What happens normally is that when eth0 connection is not present the PHY goes to sleep and stops the oscillator. Thus eth1 PHY remains without 25MHz clock. First thing you should check is this, and then program the eth0 PHY to not enter sleep mode, so that you always have 25MHz available for phy1.
  • Hi Biser,

    Yes, I work on AM335X Starter Kit, and all the ethernet data should pass through eth1 port.
    That the reason why currently ip address is not receive.
    How i program the eth0 PHY to not enter sleep mode?

    Thanks Oded.
  • That is a PHY register setting, programmed through the MDIO interface, but I'm not a software expert and can't say exactly what needs to be done.
  • Hi Biser,
    But even if eth0 is up and I try to up eth1, i receive this message: "libphy: PHY 4a101000.mdio:01 not found"
    Here is the log:

    am335x-evm login: root
    root@am335x-evm:~# ifconfig
    eth0 Link encap:Ethernet HWaddr 68:C9:0B:30:2D:54
    UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:113 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:38646 (37.7 KiB)
    Interrupt:56

    lo Link encap:Local Loopback
    inet addr:127.0.0.1 Mask:255.0.0.0
    UP LOOPBACK RUNNING MTU:65536 Metric:1
    RX packets:10 errors:0 dropped:0 overruns:0 frame:0
    TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:0
    RX bytes:700 (700.0 B) TX bytes:700 (700.0 B)

    root@am335x-evm:~# ifup eth1
    [ 1376.562462] net eth1: initializing cpsw version 1.12 (0)
    [ 1376.571399] libphy: PHY 4a101000.mdio:01 not found
    udhcpc (v1.22.1) started
    Sending discover...
    Sending discover...
    Sending discover...
    No lease, forking to background
    root@am335x-evm:~# ifconfig
    eth0 Link encap:Ethernet HWaddr 68:C9:0B:30:2D:54
    UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:143 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:48906 (47.7 KiB)
    Interrupt:56

    eth1 Link encap:Ethernet HWaddr 68:C9:0B:30:2D:56
    UP BROADCAST MULTICAST MTU:1500 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

    lo Link encap:Local Loopback
    inet addr:127.0.0.1 Mask:255.0.0.0
    UP LOOPBACK RUNNING MTU:65536 Metric:1
    RX packets:10 errors:0 dropped:0 overruns:0 frame:0
    TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:0
    RX bytes:700 (700.0 B) TX bytes:700 (700.0 B)

    root@am335x-evm:~#

    Why that?

    Thanks Oded.
  • You need to plug a network cable to eth0 to bring the PHY out of sleep.
  • Hi Biser,

    The network cable is connect and I still receive this message.
    Can I program that ethernet interface [ eth0 or eth1] will work only from P2 [ the port of eth1]?

    Thanks Oded.
  • Let's wait for comments from the Ethernet experts. They will be posted directly here when available. Meanwhile you can check this wiki: processors.wiki.ti.com/.../Linux_Core_CPSW_User's_Guide Make sure your CPSW is configured in Dual EMAC mode.
  • Hi Biser,
    Does there any answer to my problem?
    Thanks Oded.
  • Feedback will be posted directly here when available. I have information that the Ethernet team is looking into this.