Other Parts Discussed in Thread: OMAPL138
Hi
I planed to implement secure boot for our DSP board . Is C6424 support the secure boot feature ? if not I will internally mange the secure boot . My product contains of two board a security key will pass through the UART after DSP board receive the key and then decrypt the DSP image and run it . If i use this method then the boot loader shall load the decryption of the flash image . my questions
1- Is C6424 support secure boot ?
2- If not how i can customize the boot loader to support secure booting