This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

can dm8168 decoder decode



Hello all,


We are using dm8168 EZSDK 5.05.02.00 to develop decoder. We want the decoder to decode 1920x1200 video. The codec we are trying to use is H264 and the input the encoded 1920x1200 resolution at 154 Mhz pixel clock frequency.

Can the decoder decode this resolution at 60fps. if not what is the maximum resolution which the decoder can decode at 60fps.

Thanks,

Srikanth.