This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467T DVSDK3.10, building decode errors

hi,friends,

When I use make clean,make,command to build at the path /home/user/dvsdk/dvsdk_3_10_00_11/,I can get the out file.If I use the same command to build at hte path `/home/user/dvsdk/dvsdk_3_10_00_11/dvsdk_demos_3_10_00_09/dm6467/decode,produce the following information,could you give me some suggest?

[root@localhost dm6467]# cd decode
[root@localhost decode]# make clean
Removing generated files..
[root@localhost decode]# make

======== Building decode ========
Configuring application using decode.cfg

/bin/sh: /xs: No such file or directory
make: *** [decode_config/compiler.opt] Error 127

Best regards,

Xu Wenhao