This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question of GPMC and DMA of Quicklogic CSSP.

Dear all,

  QuickLogic® has developed a Customer Specific Standard Product (CSSP) to provide a camera interface bridge for the Texas Instruments Sitara AM335x processor line. Below it is the datasheet:

    www.quicklogic.com/.../QL-GPMC-CAMIF-Connect-Solution-TI-Ref-Design-Data-Sheet.pdf

   My question is:

  1. “The system must configure GPMC as 16-bit to take advantage of the DMA burst capability.”  Why? Did this mean 8-bit GPMC can't take the advantage of the DMA burst capability? The burst capability of here means the burst mode of GPMC or DMA? 

  2. "Only bit [7:0] of the GPMC bit [15:0] address/data bus is connected to valid data."  Then how did the DMA dropped the bit[15:8] while the data transfering. I mean how to set the DMA params to drop the high bits of GPMC bus? I read the source code of github and got no idea.

  Thanks, Waiting for your help.