This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x StarterWare DCAN Packet Receive example

Hi,

I am looking for AM335x Starterware DCAN example to receive the DCAN packets. I looked into dcanLpBK example but could not figure out where the DCAN packet is received?. The can_frame structure holds the int pointer to data but it doesn't point anywhere!

I understand the sequence of DCAN receive is as follows.

DCAN clock configuration

Pin mux configuration

Msg RAM initialization

Interrupt initialization and registration 

ConfigureDCAN

Invalidate All msg objects

canMsgObjectConfig for Receive

Start DCAN comminucation

Enable Interrupts (Int 0 and parity interrupt)

At this point i believe the buffer pointed to by dcan_frame structure data pointer should be filled with the Rx data.

I initialized the dcan_frame pointer to int buffer and tried this sequence, but i am not able to see any data received! (I'm sending CAN packets from RS232 to CAN converter connected to AM335x EVM)

Please suggest.