I have a problem with MMC3, which is the only one MMC on our custom board. It was "working" with SDK 1.0. With the SDK1.0 we had a problem because we don'T have any card detection pin and broken-cd didn't work. So we decided to try with the SDK 2.0 and kernel 4.1. The dts file for the MMC3 is the same in both cases:
mmc3_pins_default: pinmux_mmc3_pins {
pinctrl-single,pins = <
0x03C (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_ad15.mmc2_dat3 */
0x038 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_ad14.mmc2_dat2 */
0x034 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_ad13.mmc2_dat1 */
0x030 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_ad12.mmc2_dat0 */
0x08C (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_clk.mmc2_clk */
0x088 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_csn3.mmc2_cmd */
>;
};
&mmc3 {
status = "okay";
/* these are on the crossbar and are outlined in the
xbar-event-map element */
dmas = <&edma 12
&edma 13>;
dma-names = "tx", "rx";
bus-width = <4>;
pinctrl-names = "default";
pinctrl-0 = <&mmc3_pins_default>;
ti,needs-special-hs-handling;
ti,dual-volt;
broken-cd;
};
With the SDK 2.0 I won't get any mmcblk0p to /dev and dmesg shows the following errors for the MMC:
[ 1.253479] omap_hsmmc 47810000.mmc: GPIO lookup for consumer cd [ 1.253495] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup [ 1.253509] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@47810000[0]' [ 1.253518] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@47810000[0]' [ 1.253527] omap_hsmmc 47810000.mmc: using lookup tables for GPIO lookup [ 1.253536] omap_hsmmc 47810000.mmc: lookup for GPIO cd failed [ 1.253546] omap_hsmmc 47810000.mmc: GPIO lookup for consumer wp [ 1.253554] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup [ 1.253562] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@47810000[0]' [ 1.253570] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@47810000[0]' [ 1.253578] omap_hsmmc 47810000.mmc: using lookup tables for GPIO lookup [ 1.253585] omap_hsmmc 47810000.mmc: lookup for GPIO wp failed [ 1.254079] /ocp/mmc@47810000: voltage-ranges unspecified [ 1.289396] omap_hsmmc: probe of 47810000.mmc failed with error -22
Any ideas how I can make this work?
BR
JHi