Other Parts Discussed in Thread: AM3703
Customer is investigating changing the drive strength of AM3703 SDRAM to reduce EMI. They've tried a couple of methods of setting drive strength registers to configure drive strength to 1/8, 1/2, and full. However, they have yet to see any change to slew rate with these changes. With the latest attempt they set both of the sdrc_emr2_0 and sdrc_emr2_1 registers to 0xE0 on one unit and 0x00 on another unit to set the drive strength to 1/8th and full. When testing these units there was no change to the slew rate. Would you be able to help us figure out how to set the registers to change the drive strength of our units to full, half , 1/4th, and 1/8th? Current register values are the following.
prog_io0 - 0x0
prog_io1 - 0x100001
prog_io2 - 0x2220080
prog_io_wkup1 - 0x0
sdrc_emr2_0 - 0x20
sdrc_emr2_1 - 0x20
sdrc_Syscfg - 0x10
Thanks,
Mark