Hi - Can you please help clarify below?.
We plan on using the DM365 audio functions. I think the part can handle what we need, but I want to verify:
On the McBSP: DM365 outputs these signals, configured for 48 KHz sampling: CLKX, CLKR at 3.072 MHz FSX, FSR at 48 KHz DX with 32 bit left justified audio data, 2 channels (24 bit valid per channel) CLKOUT0 (pin T5) at 12.288 MHz Receives: DR with 32 bit left justified audio data, 2 channels (24 bit valid per channel) The assumption is that all of these frequencies can be generated in the clock generation circuit using a 27 MHz input clock. Can you let me know if these are correct assumptions?