Other Parts Discussed in Thread: OMAP-L137
I am using OMAP-L137, and use following function to copy memory by EDMA:
void EDMA_copy(int channel, Uint32 src, Uint32 dst, Uint32 nbytes)
{
edma3ccRegs->ECR |= 1 << (channel);
edma3ccRegs->SECR |= 1 << (channel);
edma3ccRegs->PARAMSET[channel].OPT =
CSL_FMKT(EDMA3CC_OPT_TCINTEN, DISABLE) |
CSL_FMKT(EDMA3CC_OPT_TCCHEN, ENABLE) |
CSL_FMKT(EDMA3CC_OPT_STATIC, STATIC) |
CSL_FMK(EDMA3CC_OPT_TCC, 0);
edma3ccRegs->PARAMSET[channel].SRC = src;
edma3ccRegs->PARAMSET[channel].DST = dst;
edma3ccRegs->PARAMSET[channel].SRC_DST_BIDX = 0;
edma3ccRegs->PARAMSET[channel].SRC_DST_CIDX = 0;
edma3ccRegs->PARAMSET[channel].LINK_BCNTRLD = 0xffff;
edma3ccRegs->PARAMSET[channel].A_B_CNT =
CSL_FMK(EDMA3CC_A_B_CNT_ACNT, nbytes) |
CSL_FMK(EDMA3CC_A_B_CNT_BCNT, 1);
edma3ccRegs->PARAMSET[channel].CCNT = 1;
edma3ccRegs->ESR |= 1 << (channel);
}
and call the function by:
EDMA_copy(0, (Uint32)srcBuffer, dst, 8);
while(1);
it copy 8 bytes from srcBuffer to dst forever.
If I add CER in Expression watch window, the bit 0 switching between 0 and 1.
If I modify some bytes in srcBuffer, the bytes in dst changed also. It seems that the EDMA repeat itself.
I want to know how to set the EDMA to copy the memory only once.