This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 TSIP clock frequency



Hi All,

I am considering the possibility to use the TSIP interface to acquire data from multiple ADCs and have the first likely naive question to start:

The clock frequency is external for TSIP, i.e. one might think it can be arbitrary. However the TSIP docs clearly state the frequency should be of fixed values (8.192 MHz, 16.384 etc). So, is it possible to use arbitrary clock frequency or the internal circuitry (like time delays etc.) really expects exact frequency values? Also, if this is the case, what are the  tolerances for exact external frequencies (like 8.192 MHz +- )?

Best Regards,

Alex