Other Parts Discussed in Thread: CCSTUDIO
Hi,
I am using the C6748 evm board and using C:\CCStudio_v3.3\bios_5_41_00_06\packages\ti\bios\examples\advanced\msgq_tsk2tsk example to test the message queue feature of the bios. I am running into a problem where the system timer some times won't start causing the example to hang. When I power cycle my evm board and restart code composurer , I get these errors in my tracing log
48957 *** ERROR: 0xc40e9180 0x4b75b099 ***
5484700 *** ERROR: 0x32a6d90 0xddbc3c3 ***
6499880 *** ERROR: 0x80c98588 0xf9ee3edb ***
7078144 *** ERROR: 0xa5825643 0x79e0ffd7 ***
43292306 *** ERROR: 0x8e08473e 0xa4fd0aa3 ***
73531581 *** ERROR: 0xe6246544 0x9bcf3930 ***
98393619 *** ERROR: 0xad5ac004 0x77e1badf ***
111157322 *** ERROR: 0x18b32876 0x98b3de9e ***
135096133 *** ERROR: 0xc122029c 0x4dfd83e7 ***
138664143 *** ERROR: 0x67399221 0xfaceb97a ***
143995060 *** ERROR: 0xb4ae1499 0xc7dadebd ***
161563337 *** ERROR: 0x5b94053e 0xffdb9fe5 ***
167854371 *** ERROR: 0xc17c5a1 0x77fbe64d ***
168734337 *** ERROR: 0xe32784ac 0xd8b9964e ***
172195463 *** ERROR: 0x1c875509 0x75d23bc7 ***
187796598 *** ERROR: 0x658a19b3 0x9fdfeeff ***
278067177 *** ERROR: 0x4c911ac0 0xa5ab57c9 ***
281266244 *** ERROR: 0x617c495 0xc7bf7232 ***
455182819 *** ERROR: 0x4498a5d1 0xe3f6fe17 ***
468746380 *** ERROR: 0xa0106143 0xf37f59b7 ***
496267580 *** ERROR: 0xa815b26a 0x9037bf70 ***
537046034 *** ERROR: 0xb723a0 0xc8d3caed ***
583008776 *** ERROR: 0x5706953c 0xb0f943bf ***
598045216 *** ERROR: 0x618c71f2 0xfd132aae ***
613517592 *** ERROR: 0xc00b5580 0x5c9f5a1b ***
633627313 *** ERROR: 0xc2920c21 0xbf81fb97 ***
637696747 *** ERROR: 0x842b61c2 0xb7f2263c ***
657980436 *** ERROR: 0x20200153 0xcefd8f93 ***
687964338 *** ERROR: 0x3b101818 0x1faadbfb ***
688937111 *** ERROR: 0xf579e574 0x8d6a277e ***
771807011 *** ERROR: 0x20316a0f 0xfb3fd31b ***
808683821 *** ERROR: 0x8712822 0xddf0f757 ***
814361288 *** ERROR: 0x930ad03f 0xbebf6305 ***
920715528 *** ERROR: 0x42200405 0x2fed3fa9 ***
964813891 *** ERROR: 0xea190006 0xdc33f68f ***
1005131523 *** ERROR: 0x80310d50 0xee9fa9f5 ***
1074766127 *** ERROR: 0x616c346d 0xbd16bba1 ***
1092646935 *** ERROR: 0x42aa1314 0x58690ff5 ***
1110081989 *** ERROR: 0x15290d89 0x2e37bad9 ***
1118846007 *** ERROR: 0xa6ea8928 0x36cf0ee5 ***
1143378881 *** ERROR: 0x734a62e3 0xecce3c7a ***
1147456405 *** ERROR: 0xd7f54ac1 0xf59a7c6d ***
1162870801 *** ERROR: 0x552a0250 0xf0577afd ***
1197415249 *** ERROR: 0x1329149 0xd3dd7dff ***
1214255636 *** ERROR: 0x7822d0d0 0x5e9a6ab1 ***
1324493313 *** ERROR: 0x209181cb 0x3353bd5a ***
1351031476 *** ERROR: 0x8687911 0x8ef9d7b9 ***
1358859944 *** ERROR: 0xfd12828d 0xbffff39a ***
1392059971 *** ERROR: 0xc0ccdc01 0x79ed54ab ***
1511396483 *** ERROR: 0x22e16a08 0xe8ebfdf3 ***
1616003071 *** ERROR: 0x1d90ac8 0xdf6f1a17 ***
1661125596 *** ERROR: 0x62b8b20c 0x8b72787e ***
1712588802 *** ERROR: 0x16a528c8 0x75ea77b6 ***
1713505458 *** ERROR: 0xe3c0f940 0x1fdcd8b7 ***
1761706249 *** ERROR: 0x9e114e04 0xedef985c ***
1769610039 *** ERROR: 0x1950855a 0xfbeb7f96 ***
1864404492 *** ERROR: 0x62a9e108 0xdbfd3e71 ***
1884856577 *** ERROR: 0x5f03404e 0xdd5f8f79 ***
1941001226 *** ERROR: 0x770a0a9 0xdfd28dff ***
2016528393 *** ERROR: 0x24453fca 0xcc8a4b9f ***
2021654879 *** ERROR: 0xba4a52fd 0x7de6dfef ***
2039150540 *** ERROR: 0x4e4318ca 0x5caf9efe ***
2042764051 *** ERROR: 0x5d350c21 0x50ff325a ***
2055755282 *** ERROR: 0x61e00008 0xfa3ff0e7 ***
When I got these errors then my system timer will start and work as normal. The project works until I start a different project, then when I switch back to this project the system timer hung again. If I repeat the cycle by powering down my evm and reconnect and get all of the above errors, then it will work again. Could you tell me what the errors are ?
Thanks.