This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3-wire spi not supported ?

Guru 20755 points

Hi,

I'm using PSP 4.1.0.2 .

I've tried to configure the driver to 3-wire but on doing that the driver fails with the following:

spi spi3.0: setup: unsupported mode bits 10
omap2_mcspi omap2_mcspi.3: can't setup spi3.0, status -22
omap2_mcspi omap2_mcspi.3: can't create new device for elbit_lcd

Is there a way to work with spi 3-wire with dm8148 ?

Best Regards,

Ran