Hi all,
The 66AK2L06 Features show that an On-chip Standalone Ram (OSR)(1MB) exists in chip. However, I can't its user manaul. Where to find it? Anyone can give me some tips? Thanks
BRs
chas
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
The 66AK2L06 Features show that an On-chip Standalone Ram (OSR)(1MB) exists in chip. However, I can't its user manaul. Where to find it? Anyone can give me some tips? Thanks
BRs
chas
As per device data manual,
The 1MB OSR is added to the device for:
• QMSS External Linking RAM
• NetCP1.5 intermediate data buffer
• Intermediate buffering of other data storage
The OSR supported features include:
• SRAM supports ECC with Read-Modify-Write logic
• RTA memory
• Support interrupt for ECC error event
• Support Little and Big-endian modes of operation
OSR does not support any type of cache access, hence this memory space must always be marked as non-cacheable region for both DSP and ARM cores.
Can you please elaborate your query? I will look for additional information and post back if i find it. Thank you.
Hi
vaibhavmahimkar said:Hello Chas,
OSR config space seems to be missing the documentation.
The register contents in that address region are identical to E CC submodule registers for GbE switch module.
www.ti.com/.../getliterature.tsp
3.5.6 ECC Submodule
Please use the above as reference while we get the documentation updated.
THank you,
Vaibhav
Hi Vaibhav,
Thanks for you kind help.
Thanks
Chas