This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linker Errors

Hello I am new to CCS6  and i am having trouble building my first project.i am using AM335x_Starterware_02_00_01_01 and  I am try to build the eneEcho project. below is the console output from the build.  I am running Windows 7  Professional any advice is appreciated.

**** Build of configuration Debug for project enetEcho ****

"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k -j 4 -s all
'Building file: C:/ti/AM335X_StarterWare_02_00_01_01/third_party/lwip-1.4.0/apps/echoserver_raw/echod.c'
'Building file: C:/ti/AM335X_StarterWare_02_00_01_01/examples/evmskAM335x/enet_echo/enetEcho.c'
'Building file: C:/ti/AM335X_StarterWare_02_00_01_01/third_party/lwip-1.4.0/ports/cpsw/lwiplib.c'
'Invoking: ARM Compiler'
'Invoking: ARM Compiler'
'Invoking: ARM Compiler'
'Finished building: C:/ti/AM335X_StarterWare_02_00_01_01/third_party/lwip-1.4.0/apps/echoserver_raw/echod.c'
' '
'Finished building: C:/ti/AM335X_StarterWare_02_00_01_01/examples/evmskAM335x/enet_echo/enetEcho.c'
' '
'Finished building: C:/ti/AM335X_StarterWare_02_00_01_01/third_party/lwip-1.4.0/ports/cpsw/lwiplib.c'
' '
'Building target: ../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/enet_echo/Debug/enetEcho.out'
'Invoking: ARM Linker'
<Linking>
error: cannot find file
   "../../../../../../../binary/armv7a/cgt_ccs/am335x/drivers/Debug/drivers.lib
   "
error: cannot find file
   "../../../../../../../binary/armv7a/cgt_ccs/am335x/system_config/Debug/syste
   m.lib"
error: cannot find file
   "../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/platform/Debu
   g/platform.lib"
error: cannot find file
   "../../../../../../../binary/armv7a/cgt_ccs/utils/Debug/utils.lib"
error: no input section is linked in

 undefined first referenced
  symbol       in file     
 --------- ----------------
 Entry                     

error: unresolved symbols remain
warning: entry-point symbol "Entry" undefined
warning: no suitable entry-point found; setting to 0
error: errors encountered during linking;
   "../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/enet_echo/Deb
   ug/enetEcho.out" not built

>> Compilation failure
gmake: *** [../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/enet_echo/Debug/enetEcho.out] Error 1
gmake: Target `all' not remade because of errors.

**** Build Finished ****