Other Parts Discussed in Thread: AM4376
We are just beginning our hardware design with the AM4376. Our desired hardware architecture utilizes asynchronous parallel NOR flash.
Our hardware design engineer is new to the AM437x family and wants to be certain of the hardware design as we work towards PCB layout.
In the AM437x Technical Reference Manual, Section 5.2.6.3.2, Tables 5-12, 5-13 and 5-14 mention a superset of signals used for interface to NOR flash memory.
Our hardware engineer wants to verify that certain signals listed in these tables are not necessary for asynchronous parallel NOR flash interface, and can be left disconnected.
We have not seen a hardware reference design for the AM437x that utilizes asynchronous parallel NOR flash. There are examples of serial (QSPI) flash interface, though, but this is not relevant to our application.
It would be helpful to know:
a) If a hardware reference design schematic is available for the AM437x utilizing asynchronous parallel NOR flash.
b) Which signals from Tables 5-12, 5-13 and 5-14 are not used for interfacing to asynchronous parallel NOR flash (to confirm that advn_ale, be0n_cle, and clk [gpmc_advn_ale, gpmc_be0n_cle, gpmc_clk] are not used).
Many thanks for the assistance.