This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

inconsistent LED behaviour during initialization



Hi, 

The LED mapping for our TI AM335x based board is as follows --

{"gpio1_15", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED1r
{"gpio1_14", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED1g
{"gpio0_27", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED2r
{"gpio0_26", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED2g
{"gpio0_23", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED3r
{"gpio0_22", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED3g
{"gpio3_17", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED4r
{"gpio3_18", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED4g
{"gpio0_20", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED5r
{"gpio0_19", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED5g
{"gpio0_10", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED6r
{"gpio3_16", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED6g
{"gpio1_13", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED7r
{"gpio1_12", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED7g
{"gpio3_15", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED8r
{"gpio3_14", OMAP_MUX_MODE7 | AM33XX_PULL_DISA | AM33XX_SLEWCTRL_SLOW}, // LED8g

The same have been done in u-boot and arch specific code of linux (3.2.0) kernel. With it, during bootup, when the u-boot hands over control to kernel, some LEDs are ON while others are OFF for a second or so, before led_init() is called.

How can we control the LED behaviour during initial part of kernel initialization code,so that all LED behaviour is consistent always?

BR,

Sourav