Other Parts Discussed in Thread: OMAPL138
Hi,
I'm using EVMC6424 and use AIS & flashburn to generate and load the hex file into the target. Our final product should contains two copies of the firmware( FW1 , FW2) stored in NAND. Normally we boot from FW1 , when firmware update take place it will wrote to FW2 and start booting from it. if booting completed successfully FW2 will overwrite FW1 and change the boot address to it's default (from FW1 ) . is it possible to customize the AIS boot load to achieve this scenario or should write my own custom bootloader
Regards,
Abdalla