Other Parts Discussed in Thread: AM4379
Hi,
We are planning to use GPMC interface of AM4379 to connect an FPGA chip in following mode.
1)NOR type Synchronous 16 bit address/data multiplexed memory device(only using AD0- 15)
2)FPGA is connnectd to Chip select 0(base address is 0x00000000)
3)FPGA CLock frequency at 50 Mhz.
To read a single data from FPGA,what are the timing parameters to be set for following?
CSWrOffTime,CSRdOffTime,CSOnTime,ADVWrOffTime,ADVRdOffTime,ADVAADMuxOnTime
ADVOnTime,WEOffTime,WEOnTime,OEOffTime,OEOnTime,rdCycleTime,wrCycleTime
rdAccessTime