Hello,
1)
My customer is planning to use AM335x Ethernet Subsystem on RMII mode.
They don't use LinuxSDK, so they are watching in the StarterWare.
But there is no RMII sample code in StarterWare. Are there any good samples of RMII ?
2)
In AM335x RMII mode, when should the IFCTL_A,IFCTL_B of MACCONTROL in CPSW_SL Registers be set ?
they are:
0 - 10Mbps operation
1 - 100Mbps operation
they should be set(1) only when link up at 100Mbps ?
Regards,
Takeshi Matsuzaki