I try to shutdown the power output of TSP65217C from AM3358. As I understood it, the RTC sub-module of AM3358 has its PMIC_POWER_EN connected to TPS65217C PWR_EN. Anyway the issue is that the RTC alarm2 will not fire when time reached, no interrupts can be seen from RTC Status Reg. In fact even the mask of alarm2 interrupt cannot be enabled in RTC Interrupt Reg. I'm using a customized Linux kernel 3.18