This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The GP19 DM6437 interrupt pin can not enter!

DM6437's GP19 pin when finished configuring edge-triggered (SET_RIS_TRIG01), the interrupt flag register (INTSTAT01) to set up, and then, the program has been into the interrupt ,clear interrupt flag bit is invalid only when clear edge trigger (CLR_RIS_TRIG01), the interrupt flag can be cleared.
The same configuration, when configured as GP98, GP55, the interrupt process is normal.

The following is the initial configuration GP19:

void Init_GP19(void)
{

CFG_PINMUX0 &= 0xFFFFFFC0;
CFG_VDD3P3V_PWDN &= 0xFFFFFFDF;

GPIO_DIR01 |= 0x80000;
GPIO_BINTEN |= 0x2;
GPIO_SET_RIS_TRIG01 |= 0x80000;
GPIO_CLR_FAL_TRIG01 |= 0x80000;
INTC_INTMUX1 &= 0xFF00FFFF;
INTC_INTMUX1 |= (73 << 16);
C64_enableIER(1<<6);
}

The following interrupt response function for the GP19:

int StateCnt = -1;
void GP19ReceiveISR(void)
{

Uint32 state;

state = GPIO_INTSTAT01 & 0x80000;
StateCnt++;

if(state == 0x80000)
{
GPIO_INTSTAT01 |= 0x80000;
if(StateCnt != 0)
{
GPIO_OUT_DATA01 &= 0xFFDFFFFF; ////POWER_EN Low
}

}

}