I'm reviving project which was originally created with CCS v3
I'm using CCS 6.1.1 on Ubuntu 15.10, and the "legacy project import" tells me it only works on Windows. Rather than go through that mess, I thought I'd just try to recreate the project from scratch.
The chip I'm using is a TMS320DM642AZNZ7
The old project file had CPUFamily=TMS320C64XX
In CCS 6.1.1, Project Properties, General, Main, Device, I don't see any "Variant" that matches this processor.
What do I use?