This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL137 with 16C554 8x serial port expand and CPLD



Hi

Recently I am working with a project. I design  a 8x serial communication port board to use with OMAPL137 DSP board.

I used two ST16C554, each with 4 serial port, so total 8 serial port there and the 8x interrupts of ST16C554 are combine into to two interrrupts to DSP by CPLD

The two interrupt to DSP are connected to EMA_D[8], EMA_D[9] respectively.

The 8 bytes data bus from ST16C554 are connected to EMA_D[0] -- EMA_D[7] respectively.

These serial port base address are mapped to EMIFA base address.

Now I can send data and receive date through the serial port by continuely monitor the serial port register status.

I want to use interrupt to handle the serial port event and send and receive data.

I have setup the EMA_D[8], EMA_D[9] by PINMUX register as GPIO0[8] and GPIO[9].

and configed the event 65 (which is for GPIO interrupt ? ) through TCF as default interrupt handler

I use HWI 8 for  event 65 .

Now the problem is the interrup could not be get called.

Is it right that I do ? How should I do the next ?

I would be really grateful for your help

Please forgive my bad english.

Thanks