This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[AM572x] Using VOUT2 for 24-bit DPI output

Other Parts Discussed in Thread: SN65LVDS93

Hello:

I am working with our custom hardware that uses VOUT2 (not VOUT1 like the EVM) to output graphics to our LCD panel. Unfortunately, I am unable to display anything on it.

It doesn't appear that LCD2/VOUT2 is completely implemented yet. Is that correct?

 

Background:

Our hardware routes the appropriate VOUT2 signals directly from the AM572x processor to an SN65LVDS93 LVDS transmitter, and the LVDS output goes to our display connector along with an LCD enable signal (GPIO) and PWM backlight (ehrpwm1a).

The display turns on and rotates through color test images (primary colors and checkerboard). The colors look good. The backlight brightness is adjustable as expected.

My software is based on the recently released Linux SDK2.0.0.0 and the dts configuration for my display is below:

/ {
aliases {
display0 = &lcd0;
display1 = &hdmi0;
};
backlight: backlight { status = "okay"; compatible = "pwm-backlight"; brightness-levels = <0 4 8 16 32 64 128 255>; default-brightness-level = <6>; }; lcd0: display { status = "okay"; compatible = "ETM0700G0DH6", "panel-dpi"; pinctrl-names = "default"; pinctrl-0 = <&lcd_pins &display_en_pin>; enable-gpios = <&gpio8 23 GPIO_ACTIVE_LOW>; label = "lcd2"; panel-timing { clock-frequency = <40000000>; hactive = <800>; vactive = <480>; hfront-porch = <40>; hback-porch = <216>; hsync-len = <128>; vback-porch = <35>; vfront-porch = <10>; vsync-len = <2>; hsync-active = <1>; vsync-active = <1>; de-active = <1>; pixelclk-active = <1>; }; port { lcd_in: endpoint { remote-endpoint = <&dpi_out>; }; }; }; }; &dss { ports { #address-cells = <1>; #size-cells = <0>; port { reg = <1>; dpi_out: endpoint { remote-endpoint = <&lcd_in>; data-lines = <24>; }; }; }; };

Debug

I have modified drivers/video/fbdev/omap2/dss/dss.c:dss_dpi_select_source_dra7xx() to select the source appropriately for OMAP_DSS_CHANNEL_LCD2 in addition to OMAP_DSS_CHANNEL_LCD, and although it set DSS_CTRL to select LCD2 as the parallel output, it did not resolve any of the errors I am seeing. Also, the debugfs omapdss clk output is showing that there is no pclk or lclk set for LCD2, but I can't find anything in particular that explains why the PLL wouldn't be configured correctly. If I configure the lcd0 port to use reg = <0>, which corresponds to OMAP_DSS_CHANNEL_LCD and is not supported for VOUT2, the LCD1 channel has the proper 40Mhz pclk I am setting, LCD2 channel has the DSS_FCK, and I see no errors. But of course that does not output anything on VOUT2.

Furthermore, I am seeing 

[ 2.421133] omapdrm omapdrm.0: lcd2: timeout waiting for enable
[ 2.471129] omapdrm omapdrm.0: atomic complete timeout (pipe 1)!

during boot, and am hitting a couple BUG_ON scenarios related to the DISPC_CONTROL2.GOWB register bit (as seen in attached the kernel_boot.log).

My results are the same with or without HDMI configured.

Any thoughts? I have been going over the registers and before I dive even deeper, I'm hoping for additional input.

Thanks,

Russell Robinson

kernel_boot.log

# cat /sys/kernel/debug/omapdss/dss
DSS_REVISION                        00000061
DSS_SYSCONFIG                       00000000
DSS_SYSSTATUS                       00000001
DSS_CONTROL                         00021000
# cat /sys/kernel/debug/omapdss/clk
- DSS -
DSS_FCK (DSS_CLK) = 192000000
- DISPC -
dispc fclk source = DSS_FCK (DSS_CLK)
fck             192000000
- DISPC-CORE-CLK -
lck             192000000       lck div 1
- LCD -
LCD clk source = DSS_FCK (DSS_CLK)
lck             48000000        lck div 4
pck             48000000        pck div 1
- LCD2 -
LCD2 clk source = DSI_PLL2_HSDIV_DISPC (DPLL_DSI1_C_CLK1)
lck             0               lck div 1
pck             0               pck div 1
- LCD3 -
LCD3 clk source = DSS_FCK (DSS_CLK)
lck             48000000        lck div 4
pck             48000000        pck div 1
# cat /sys/kernel/debug/omapdss/dispc
DISPC_REVISION                                     00000051
DISPC_SYSCONFIG                                    00002015
DISPC_SYSSTATUS                                    00000001
DISPC_IRQSTATUS                                    00000000
DISPC_IRQENABLE                                    0016964c
DISPC_CONTROL                                      00018002
DISPC_CONFIG                                       00000004
DISPC_CAPABLE                                      00000000
DISPC_LINE_STATUS                                  00000000
DISPC_LINE_NUMBER                                  00000000
DISPC_GLOBAL_ALPHA                                 ffffffff
DISPC_CONTROL2                                     00000329
DISPC_CONFIG2                                      00000000
DISPC_CONTROL3                                     00000000
DISPC_CONFIG3                                      00000000
DISPC_GLOBAL_MFLAG_ATTRIBUTE                       00000001
DISPC_DEFAULT_COLOR(LCD)                           00000000
DISPC_TRANS_COLOR(LCD)                             00000000
DISPC_SIZE_MGR(LCD)                                00000000
DISPC_TIMING_H(LCD)                                00000000
DISPC_TIMING_V(LCD)                                00000000
DISPC_POL_FREQ(LCD)                                00000000
DISPC_DIVISORo(LCD)                                00040001
DISPC_DATA_CYCLE1(LCD)                             00000000
DISPC_DATA_CYCLE2(LCD)                             00000000
DISPC_DATA_CYCLE3(LCD)                             00000000
DISPC_CPR_COEF_R(LCD)                              00000000
DISPC_CPR_COEF_G(LCD)                              00000000
DISPC_CPR_COEF_B(LCD)                              00000000
DISPC_DEFAULT_COLOR(TV)                            00000000
DISPC_TRANS_COLOR(TV)                              00000000
DISPC_SIZE_MGR(TV)                                 0437077f
DISPC_DEFAULT_COLOR(LCD2)                          00000000
DISPC_TRANS_COLOR(LCD2)                            00000000
DISPC_SIZE_MGR(LCD2)                               01df031f
DISPC_TIMING_H(LCD2)                               0d70277f
DISPC_TIMING_V(LCD2)                               02300a01
DISPC_POL_FREQ(LCD2)                               00030000
DISPC_DIVISORo(LCD2)                               00010001
DISPC_DATA_CYCLE1(LCD2)                            00000000
DISPC_DATA_CYCLE2(LCD2)                            00000000
DISPC_DATA_CYCLE3(LCD2)                            00000000
DISPC_CPR_COEF_R(LCD2)                             00000000
DISPC_CPR_COEF_G(LCD2)                             00000000
DISPC_CPR_COEF_B(LCD2)                             00000000
DISPC_DEFAULT_COLOR(LCD3)                          00000000
DISPC_TRANS_COLOR(LCD3)                            00000000
DISPC_SIZE_MGR(LCD3)                               00000000
DISPC_TIMING_H(LCD3)                               00000000
DISPC_TIMING_V(LCD3)                               00000000
DISPC_POL_FREQ(LCD3)                               00000000
DISPC_DIVISORo(LCD3)                               00040001
DISPC_DATA_CYCLE1(LCD3)                            00000000
DISPC_DATA_CYCLE2(LCD3)                            00000000
DISPC_DATA_CYCLE3(LCD3)                            00000000
DISPC_CPR_COEF_R(LCD3)                             00000000
DISPC_CPR_COEF_G(LCD3)                             00000000
DISPC_CPR_COEF_B(LCD3)                             00000000
DISPC_OVL_BA0(GFX)                                 7efa7000
DISPC_OVL_BA1(GFX)                                 7efa7000
DISPC_OVL_POSITION(GFX)                            00000000
DISPC_OVL_SIZE(GFX)                                0437077f
DISPC_OVL_ATTRIBUTES(GFX)                          02004191
DISPC_OVL_FIFO_THRESHOLD(GFX)                      07ff07f8
DISPC_OVL_FIFO_SIZE_STATUS(GFX)                    00000500
DISPC_OVL_ROW_INC(GFX)                             00000001
DISPC_OVL_PIXEL_INC(GFX)                           00000001
DISPC_OVL_PRELOAD(GFX)                             000007ff
DISPC_OVL_MFLAG_THRESHOLD(GFX)                     05000400
DISPC_OVL_WINDOW_SKIP(GFX)                         00000000
DISPC_OVL_TABLE_BA(GFX)                            00000000
DISPC_OVL_BA0(VID1)                                7ee30000
DISPC_OVL_BA1(VID1)                                7ee30000
DISPC_OVL_POSITION(VID1)                           00000000
DISPC_OVL_SIZE(VID1)                               01df031f
DISPC_OVL_ATTRIBUTES(VID1)                         42a08011
DISPC_OVL_FIFO_THRESHOLD(VID1)                     07ff07f8
DISPC_OVL_FIFO_SIZE_STATUS(VID1)                   00000800
DISPC_OVL_ROW_INC(VID1)                            00000001
DISPC_OVL_PIXEL_INC(VID1)                          00000001
DISPC_OVL_PRELOAD(VID1)                            000007ff
DISPC_OVL_MFLAG_THRESHOLD(VID1)                    05000400
DISPC_OVL_FIR(VID1)                                04000400
DISPC_OVL_PICTURE_SIZE(VID1)                       01df031f
DISPC_OVL_ACCU0(VID1)                              00000000
DISPC_OVL_ACCU1(VID1)                              00000000
DISPC_OVL_BA0_UV(VID1)                             00000000
DISPC_OVL_BA1_UV(VID1)                             00000000
DISPC_OVL_FIR2(VID1)                               04000400
DISPC_OVL_ACCU2_0(VID1)                            00000000
DISPC_OVL_ACCU2_1(VID1)                            00000000
DISPC_OVL_ATTRIBUTES2(VID1)                        00000000
DISPC_OVL_BA0(VID2)                                00000000
DISPC_OVL_BA1(VID2)                                00000000
DISPC_OVL_POSITION(VID2)                           00000000
DISPC_OVL_SIZE(VID2)                               00000000
DISPC_OVL_ATTRIBUTES(VID2)                         02808400
DISPC_OVL_FIFO_THRESHOLD(VID2)                     07ff07f8
DISPC_OVL_FIFO_SIZE_STATUS(VID2)                   00000800
DISPC_OVL_ROW_INC(VID2)                            00000001
DISPC_OVL_PIXEL_INC(VID2)                          00000001
DISPC_OVL_PRELOAD(VID2)                            000007ff
DISPC_OVL_MFLAG_THRESHOLD(VID2)                    05000400
DISPC_OVL_FIR(VID2)                                04000400
DISPC_OVL_PICTURE_SIZE(VID2)                       00000000
DISPC_OVL_ACCU0(VID2)                              00000000
DISPC_OVL_ACCU1(VID2)                              00000000
DISPC_OVL_BA0_UV(VID2)                             00000000
DISPC_OVL_BA1_UV(VID2)                             00000000
DISPC_OVL_FIR2(VID2)                               04000400
DISPC_OVL_ACCU2_0(VID2)                            00000000
DISPC_OVL_ACCU2_1(VID2)                            00000000
DISPC_OVL_ATTRIBUTES2(VID2)                        00000000
DISPC_OVL_BA0(VID3)                                00000000
DISPC_OVL_BA1(VID3)                                00000000
DISPC_OVL_POSITION(VID3)                           00000000
DISPC_OVL_SIZE(VID3)                               00000000
DISPC_OVL_ATTRIBUTES(VID3)                         02808400
DISPC_OVL_FIFO_THRESHOLD(VID3)                     07ff07f8
DISPC_OVL_FIFO_SIZE_STATUS(VID3)                   00000800
DISPC_OVL_ROW_INC(VID3)                            00000001
DISPC_OVL_PIXEL_INC(VID3)                          00000001
DISPC_OVL_PRELOAD(VID3)                            000007ff
DISPC_OVL_MFLAG_THRESHOLD(VID3)                    05000400
DISPC_OVL_FIR(VID3)                                04000400
DISPC_OVL_PICTURE_SIZE(VID3)                       00000000
DISPC_OVL_ACCU0(VID3)                              00000000
DISPC_OVL_ACCU1(VID3)                              00000000
DISPC_OVL_BA0_UV(VID3)                             00000000
DISPC_OVL_BA1_UV(VID3)                             00000000
DISPC_OVL_FIR2(VID3)                               04000400
DISPC_OVL_ACCU2_0(VID3)                            00000000
DISPC_OVL_ACCU2_1(VID3)                            00000000
DISPC_OVL_ATTRIBUTES2(VID3)                        00000000
DISPC_OVL_FIR_COEF_H_0(VID1)                       00800000
DISPC_OVL_FIR_COEF_H_1(VID1)                       0e7df601
DISPC_OVL_FIR_COEF_H_2(VID1)                       2172f102
DISPC_OVL_FIR_COEF_H_3(VID1)                       3762f001
DISPC_OVL_FIR_COEF_H_4(VID1)                       f24e4ef2
DISPC_OVL_FIR_COEF_H_5(VID1)                       f06237f6
DISPC_OVL_FIR_COEF_H_6(VID1)                       f17221fa
DISPC_OVL_FIR_COEF_H_7(VID1)                       f67d0efe
DISPC_OVL_FIR_COEF_HV_0(VID1)                      00800000
DISPC_OVL_FIR_COEF_HV_1(VID1)                      0e7df6fe
DISPC_OVL_FIR_COEF_HV_2(VID1)                      2172f1fa
DISPC_OVL_FIR_COEF_HV_3(VID1)                      3762f0f6
DISPC_OVL_FIR_COEF_HV_4(VID1)                      f24e4e00
DISPC_OVL_FIR_COEF_HV_5(VID1)                      f0623701
DISPC_OVL_FIR_COEF_HV_6(VID1)                      f1722102
DISPC_OVL_FIR_COEF_HV_7(VID1)                      f67d0e01
DISPC_OVL_CONV_COEF_0(VID1)                        0199012a
DISPC_OVL_CONV_COEF_1(VID1)                        012a0000
DISPC_OVL_CONV_COEF_2(VID1)                        079c0730
DISPC_OVL_CONV_COEF_3(VID1)                        0000012a
DISPC_OVL_CONV_COEF_4(VID1)                        00000205
DISPC_OVL_FIR_COEF_V_0(VID1)                       00000000
DISPC_OVL_FIR_COEF_V_1(VID1)                       0000fe01
DISPC_OVL_FIR_COEF_V_2(VID1)                       0000fa02
DISPC_OVL_FIR_COEF_V_3(VID1)                       0000f601
DISPC_OVL_FIR_COEF_V_4(VID1)                       000000f2
DISPC_OVL_FIR_COEF_V_5(VID1)                       000001f6
DISPC_OVL_FIR_COEF_V_6(VID1)                       000002fa
DISPC_OVL_FIR_COEF_V_7(VID1)                       000001fe
DISPC_OVL_FIR_COEF_H2_0(VID1)                      00000000
DISPC_OVL_FIR_COEF_H2_1(VID1)                      00000000
DISPC_OVL_FIR_COEF_H2_2(VID1)                      00000000
DISPC_OVL_FIR_COEF_H2_3(VID1)                      00000000
DISPC_OVL_FIR_COEF_H2_4(VID1)                      00000000
DISPC_OVL_FIR_COEF_H2_5(VID1)                      00000000
DISPC_OVL_FIR_COEF_H2_6(VID1)                      00000000
DISPC_OVL_FIR_COEF_H2_7(VID1)                      00000000
DISPC_OVL_FIR_COEF_HV2_0(VID1)                     00000000
DISPC_OVL_FIR_COEF_HV2_1(VID1)                     00000000
DISPC_OVL_FIR_COEF_HV2_2(VID1)                     00000000
DISPC_OVL_FIR_COEF_HV2_3(VID1)                     00000000
DISPC_OVL_FIR_COEF_HV2_4(VID1)                     00000000
DISPC_OVL_FIR_COEF_HV2_5(VID1)                     00000000
DISPC_OVL_FIR_COEF_HV2_6(VID1)                     00000000
DISPC_OVL_FIR_COEF_HV2_7(VID1)                     00000000
DISPC_OVL_FIR_COEF_V2_0(VID1)                      00000000
DISPC_OVL_FIR_COEF_V2_1(VID1)                      00000000
DISPC_OVL_FIR_COEF_V2_2(VID1)                      00000000
DISPC_OVL_FIR_COEF_V2_3(VID1)                      00000000
DISPC_OVL_FIR_COEF_V2_4(VID1)                      00000000
DISPC_OVL_FIR_COEF_V2_5(VID1)                      00000000
DISPC_OVL_FIR_COEF_V2_6(VID1)                      00000000
DISPC_OVL_FIR_COEF_V2_7(VID1)                      00000000
DISPC_OVL_FIR_COEF_H_0(VID2)                       00000000
DISPC_OVL_FIR_COEF_H_1(VID2)                       00000000
DISPC_OVL_FIR_COEF_H_2(VID2)                       00000000
DISPC_OVL_FIR_COEF_H_3(VID2)                       00000000
DISPC_OVL_FIR_COEF_H_4(VID2)                       00000000
DISPC_OVL_FIR_COEF_H_5(VID2)                       00000000
DISPC_OVL_FIR_COEF_H_6(VID2)                       00000000
DISPC_OVL_FIR_COEF_H_7(VID2)                       00000000
DISPC_OVL_FIR_COEF_HV_0(VID2)                      00000000
DISPC_OVL_FIR_COEF_HV_1(VID2)                      00000000
DISPC_OVL_FIR_COEF_HV_2(VID2)                      00000000
DISPC_OVL_FIR_COEF_HV_3(VID2)                      00000000
DISPC_OVL_FIR_COEF_HV_4(VID2)                      00000000
DISPC_OVL_FIR_COEF_HV_5(VID2)                      00000000
DISPC_OVL_FIR_COEF_HV_6(VID2)                      00000000
DISPC_OVL_FIR_COEF_HV_7(VID2)                      00000000
DISPC_OVL_CONV_COEF_0(VID2)                        0199012a
DISPC_OVL_CONV_COEF_1(VID2)                        012a0000
DISPC_OVL_CONV_COEF_2(VID2)                        079c0730
DISPC_OVL_CONV_COEF_3(VID2)                        0000012a
DISPC_OVL_CONV_COEF_4(VID2)                        00000205
DISPC_OVL_FIR_COEF_V_0(VID2)                       00000000
DISPC_OVL_FIR_COEF_V_1(VID2)                       00000000
DISPC_OVL_FIR_COEF_V_2(VID2)                       00000000
DISPC_OVL_FIR_COEF_V_3(VID2)                       00000000
DISPC_OVL_FIR_COEF_V_4(VID2)                       00000000
DISPC_OVL_FIR_COEF_V_5(VID2)                       00000000
DISPC_OVL_FIR_COEF_V_6(VID2)                       00000000
DISPC_OVL_FIR_COEF_V_7(VID2)                       00000000
DISPC_OVL_FIR_COEF_H2_0(VID2)                      00000000
DISPC_OVL_FIR_COEF_H2_1(VID2)                      00000000
DISPC_OVL_FIR_COEF_H2_2(VID2)                      00000000
DISPC_OVL_FIR_COEF_H2_3(VID2)                      00000000
DISPC_OVL_FIR_COEF_H2_4(VID2)                      00000000
DISPC_OVL_FIR_COEF_H2_5(VID2)                      00000000
DISPC_OVL_FIR_COEF_H2_6(VID2)                      00000000
DISPC_OVL_FIR_COEF_H2_7(VID2)                      00000000
DISPC_OVL_FIR_COEF_HV2_0(VID2)                     00000000
DISPC_OVL_FIR_COEF_HV2_1(VID2)                     00000000
DISPC_OVL_FIR_COEF_HV2_2(VID2)                     00000000
DISPC_OVL_FIR_COEF_HV2_3(VID2)                     00000000
DISPC_OVL_FIR_COEF_HV2_4(VID2)                     00000000
DISPC_OVL_FIR_COEF_HV2_5(VID2)                     00000000
DISPC_OVL_FIR_COEF_HV2_6(VID2)                     00000000
DISPC_OVL_FIR_COEF_HV2_7(VID2)                     00000000
DISPC_OVL_FIR_COEF_V2_0(VID2)                      00000000
DISPC_OVL_FIR_COEF_V2_1(VID2)                      00000000
DISPC_OVL_FIR_COEF_V2_2(VID2)                      00000000
DISPC_OVL_FIR_COEF_V2_3(VID2)                      00000000
DISPC_OVL_FIR_COEF_V2_4(VID2)                      00000000
DISPC_OVL_FIR_COEF_V2_5(VID2)                      00000000
DISPC_OVL_FIR_COEF_V2_6(VID2)                      00000000
DISPC_OVL_FIR_COEF_V2_7(VID2)                      00000000
DISPC_OVL_FIR_COEF_H_0(VID3)                       00000000
DISPC_OVL_FIR_COEF_H_1(VID3)                       00000000
DISPC_OVL_FIR_COEF_H_2(VID3)                       00000000
DISPC_OVL_FIR_COEF_H_3(VID3)                       00000000
DISPC_OVL_FIR_COEF_H_4(VID3)                       00000000
DISPC_OVL_FIR_COEF_H_5(VID3)                       00000000
DISPC_OVL_FIR_COEF_H_6(VID3)                       00000000
DISPC_OVL_FIR_COEF_H_7(VID3)                       00000000
DISPC_OVL_FIR_COEF_HV_0(VID3)                      00000000
DISPC_OVL_FIR_COEF_HV_1(VID3)                      00000000
DISPC_OVL_FIR_COEF_HV_2(VID3)                      00000000
DISPC_OVL_FIR_COEF_HV_3(VID3)                      00000000
DISPC_OVL_FIR_COEF_HV_4(VID3)                      00000000
DISPC_OVL_FIR_COEF_HV_5(VID3)                      00000000
DISPC_OVL_FIR_COEF_HV_6(VID3)                      00000000
DISPC_OVL_FIR_COEF_HV_7(VID3)                      00000000
DISPC_OVL_CONV_COEF_0(VID3)                        0199012a
DISPC_OVL_CONV_COEF_1(VID3)                        012a0000
DISPC_OVL_CONV_COEF_2(VID3)                        079c0730
DISPC_OVL_CONV_COEF_3(VID3)                        0000012a
DISPC_OVL_CONV_COEF_4(VID3)                        00000205
DISPC_OVL_FIR_COEF_V_0(VID3)                       00000000
DISPC_OVL_FIR_COEF_V_1(VID3)                       00000000
DISPC_OVL_FIR_COEF_V_2(VID3)                       00000000
DISPC_OVL_FIR_COEF_V_3(VID3)                       00000000
DISPC_OVL_FIR_COEF_V_4(VID3)                       00000000
DISPC_OVL_FIR_COEF_V_5(VID3)                       00000000
DISPC_OVL_FIR_COEF_V_6(VID3)                       00000000
DISPC_OVL_FIR_COEF_V_7(VID3)                       00000000
DISPC_OVL_FIR_COEF_H2_0(VID3)                      00000000
DISPC_OVL_FIR_COEF_H2_1(VID3)                      00000000
DISPC_OVL_FIR_COEF_H2_2(VID3)                      00000000
DISPC_OVL_FIR_COEF_H2_3(VID3)                      00000000
DISPC_OVL_FIR_COEF_H2_4(VID3)                      00000000
DISPC_OVL_FIR_COEF_H2_5(VID3)                      00000000
DISPC_OVL_FIR_COEF_H2_6(VID3)                      00000000
DISPC_OVL_FIR_COEF_H2_7(VID3)                      00000000
DISPC_OVL_FIR_COEF_HV2_0(VID3)                     00000000
DISPC_OVL_FIR_COEF_HV2_1(VID3)                     00000000
DISPC_OVL_FIR_COEF_HV2_2(VID3)                     00000000
DISPC_OVL_FIR_COEF_HV2_3(VID3)                     00000000
DISPC_OVL_FIR_COEF_HV2_4(VID3)                     00000000
DISPC_OVL_FIR_COEF_HV2_5(VID3)                     00000000
DISPC_OVL_FIR_COEF_HV2_6(VID3)                     00000000
DISPC_OVL_FIR_COEF_HV2_7(VID3)                     00000000
DISPC_OVL_FIR_COEF_V2_0(VID3)                      00000000
DISPC_OVL_FIR_COEF_V2_1(VID3)                      00000000
DISPC_OVL_FIR_COEF_V2_2(VID3)                      00000000
DISPC_OVL_FIR_COEF_V2_3(VID3)                      00000000
DISPC_OVL_FIR_COEF_V2_4(VID3)                      00000000
DISPC_OVL_FIR_COEF_V2_5(VID3)                      00000000
DISPC_OVL_FIR_COEF_V2_6(VID3)                      00000000
DISPC_OVL_FIR_COEF_V2_7(VID3)                      00000000