How to enable ethernet connection to host system? Physical link seems up but no ip number.
See teminal output below:
ROOT@AM335X-EVM:~# [ 2099.458312] PHY: 0:00 - Link is Up - 1000/Full
[ 2101.458343] PHY: 0:00 - Link is Down
[ 2109.458343] PHY: 0:00 - Link is Up - 1000/Full
ROOT@AM335X-EVM:~# IP ADDR
1: LO: <LOOPBACK,UP,LOWER_UP> MTU 16436 QDISC NOQUEUE STATE UNKNOWN
LINK/LOOPBACK 00:00:00:00:00:00 BRD 00:00:00:00:00:00
INET 127.0.0.1/8 SCOPE HOST LO
PS
I have no MATRIX interface control because the touch screen doesn't work ( I recalibrated it to no effect) therefore cannot go to Network Settings icon from the Settings Submenu.