This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6727 boot problems

 

i use parallel FLASH mode to boot my code as the documents "Using the TMS320C672x Bootloader" says. I use  BIOS  In my project , there have a problems is that BIOS generat a .cmd  document and the Bootloader have a .cmd ,too.when i bild this project there have error like this:

<Linking>
>> F:\\DSP\\DPD\\DPD_project_LS_boot\\TISecondaryBootlnk.cmd, line 59: warning:
               multiple definitions of SECTION named '.stack'
>>   error: memory types IRAM and IRAM on page 0 overlap
>>   error: memory types SDRAM and SDRAM on page 0 overlap
>> F:\\DSP\\DPD\\DPD_project_LS_boot\\TISecondaryBootlnk.cmd, line 69: warning:
               (appPage0) not found
>> F:\\DSP\\DPD\\DPD_project_LS_boot\\TISecondaryBootlnk.cmd, line 73: warning:
               (fill1) not found
>> F:\\DSP\\DPD\\DPD_project_LS_boot\\TISecondaryBootlnk.cmd, line 74: warning:
               (appPage1) not found
>> F:\\DSP\\DPD\\DPD_project_LS_boot\\TISecondaryBootlnk.cmd, line 75: warning:
               (fill2) not found
>> F:\\DSP\\DPD\\DPD_project_LS_boot\\TISecondaryBootlnk.cmd, line 77: warning:
               (appPage2) not found
>> F:\\DSP\\DPD\\DPD_project_LS_boot\\TISecondaryBootlnk.cmd, line 78: warning:
               (fill3) not found
>> F:\\DSP\\DPD\\DPD_project_LS_boot\\TISecondaryBootlnk.cmd, line 79: warning:
               (apptext) not found
>> warning: creating output section .printf without SECTIONS specification
>> warning: can't create map file 'o./Debug/DPD_project_2.out': No such file or
            directory
>>   error: errors in input - a.out not built

>> Compilation failure

Build Complete,
  4 Errors, 10 Warnings, 0 Remarks.


What should i do ?

Thank you very much for answer my question. this problem has bother me a week~~~