This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 - speed grade identification?

Hi,

Can you help clarify if there is a register in the dm36x that provides the device speed grade rating of the chip, and example: 400 MHz vs 297 MHz?

I found  the Device ID register in the System Module section, but this does not have a field defined for device speed grade.Looking in sprz294d.pdf, section 1.2 Revision Identification describes the device markings, but is there a way to determine this when running code?