This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 and TPS6590 in 2.6.32 Kernel (VMMC1 Control)

Expert 1070 points


Hello,

 

I have a custom 3530 board running the TPS6590 power chip and the 2.6.32 linux kernel.  I have noticed the VMMC1 voltage is toggling

between the 3.15V level and the 3.0V level.  This toggle can last 2 or 3 seconds at a time. 

 

Has anyone seen this?  Is there some type of power control going on in the kernel I don't know about?

 

Thanks.