Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hello,
I would like to set up a build environment for OMAP-L138 software on a headless Ubuntu 14.04 LTS Server. I have already set up CCS on a Ubuntu desktop system, and that is working fine.
The server is command line only -- it doesn't have the GUI desktop. Building for the ARM should not be a problem -- I already have the Linux cross-compiler installed for that.
The DSP build environment, however, is giving me problems. Is there a way to use the TI bin installers for XDC Tools and SYS/BIOS that do not require the GUI environment? Are there separate installers (other than the bin installers) that are needed?
The product we are building uses xdctools_3_25_03_72, bios_5_42_01_09, and c6000_7.4.4. Is there anything else needed for installing and using the DSP compilers on a headless Linux server?
Thanks for your help.
Regards,
Ben