Hello, I am using the following MP3 codec from TI:
c64xplus_mp3dec_1_31_001_production
The datasheet in the release gives some MIPS measurements on a DM644x EVM for some sample mp3 files. It gives the average value for fl11.mp3 as about 15 MHz. On my DA830 DSK, the test application under CCSv4 and RTSC gives an average of 23 MHz.
Is this type of difference with the same code (cache management, etc) expected between these processors?
Thanks
David Kelly