Hi, I have a question about AM437x DDR3 memory placement. We are using two 16-bit DDR3L devices arranged as one 32-bit bank. Which DDR3L memory should be placed near to processor? Lower data byte or higher data byte? Or is it irrespective which DDR3L memory is placed near to processor? In AM437x datasheet(sprs851b) page.176 Figure 5-52, 16bit DDR3 of Lower data byte are placed near to the processor. But in page.195 Figure 5-77, DDR3 of Lowest data byte are placed farest to the processor, and Highest data byte are placed nearest to the processor. So, I guess it is irrespective which DDR3 chip is placed near to processor. best regards, g.f.