Other Parts Discussed in Thread: TMS320C6455
Sir,
In my board there is TMS320C6455 and i connect xds 510usb plus emulator but below error is comming.
and
Trouble Reading Memory Block at 0xa0000004 on Page 0 of Length 0x1:
Error 0x00000002/-1202
Error during: Memory,
CPU pipeline is stalled and the CPU is 'not ready'. This means
that the CPU has performed an access which has not
completed, and the CPU is waiting. The target may need to be
reset. The user can choose 'Yes' to force the CPU to be 'ready'.
When this is done, the user will have the ability to examine
the target memory and registers to determine the cause of the
CPU stall. If CPU hang is caused by application and it has been
forced to be 'ready', the CPU should not be run without a reset.
Yes - force CPU ready (might corrupt the code)
Disconnect - disconnect CCS so that it can be reset
Retry - attempt the command again
Sequence ID: 69
Error Code: -1202
Error Class: 0x00000002
how to solve this error. we are not using external flash memory right now. so is there any issue because of flash memory.