Hi,
Can we cross compile openOCD for DM8140 with Linux board?
I have tried to cross compiling the openOCD for DM8148 with Linux board, but while configuring it was checking for arm-none-linux-gnueabi-g77 etc. and it was not getting the link to the file.
Error log:
checking for arm-none-linux-gnueabi-g77... no
checking for arm-none-linux-gnueabi-f77... no
checking for arm-none-linux-gnueabi-xlf... no
checking for arm-none-linux-gnueabi-frt... no
checking for arm-none-linux-gnueabi-pgf77... no
checking for arm-none-linux-gnueabi-fort77... no
checking for arm-none-linux-gnueabi-fl32... no
checking for arm-none-linux-gnueabi-af77... no
checking for arm-none-linux-gnueabi-f90... no
checking for arm-none-linux-gnueabi-xlf90... no
checking for arm-none-linux-gnueabi-pgf90... no
checking for arm-none-linux-gnueabi-epcf90... no
checking for arm-none-linux-gnueabi-f95... no
checking for arm-none-linux-gnueabi-fort... no
checking for arm-none-linux-gnueabi-xlf95... no
checking for arm-none-linux-gnueabi-ifc... no
checking for arm-none-linux-gnueabi-efc... no
checking for arm-none-linux-gnueabi-pgf95... no
checking for arm-none-linux-gnueabi-lf95... no
checking for arm-none-linux-gnueabi-gfortran... no
checking for g77... no
checking for f77... no
checking for xlf... no
checking for frt... no
checking for pgf77... no
checking for fort77... no
checking for fl32... no
checking for af77... no
checking for f90... no
checking for xlf90... no
checking for pgf90... no
checking for epcf90... no
checking for f95... no
checking for fort... no
checking for xlf95... no
checking for ifc... no
checking for efc... no
checking for pgf95... no
checking for lf95... no
checking for gfortran... no
checking whether we are using the GNU Fortran 77 compiler... no
checking whether accepts -g... no
checking the maximum length of command line arguments... 32768
checking command to parse /home/arm2010q1_alsa/bin//arm-none-linux-gnueabi-nm -B output from arm-none-linux-gnueabi-gcc object... ok
checking for objdir... .libs
Thanks,
Sudheer.