Hello all,
I am trying to run TcpEcho example, but I'm facing some issues that I can't run properly.
First I was trying to connect via DCHP as original procedure, but I get the same error F002 already posted here acouple months ago.
I have checked the TM2C129 Emac issue and looks like the TI-RTOS TivaC version I am using (2.14.00.10) has already updated the EMACsnow.c file with the working around. I have also installed on my PC a DCHP server, so I don't understand where can be the problem
I also tried to use an static IP, changing it on .cfg file. I went a little bit further, now I can create a socket, bind it and connect it. Once the tcpHandler create a thread and call task tcpWorker, I get -1 as result of recv() call. Tried also to monitor the error by using fdError() function and the result is also -1, which is not mentioned for recv() function as a error result.
Please, anyone has a hint how could I go around this issue?
Thank you in advance.
Bests,
Douglas