Hi,
We are pleased to announce the release of our new WEC2013 BSP for TI AM57x. You can already try it out here :
www.adeneo-embedded.com/.../17409
The WEC2013 reference board support package for AM57x includes the features listed down below :
| Features | Status | Comment |
| Display/Graphics | Yes |
|
| Displays | Yes |
|
| Touchscreen | Yes | |
| USB host | Yes | |
| USB Function | No | |
| PCIe | Yes | |
| SATA | Yes | |
| PRU | Yes | |
| eMMC | Yes | |
|
SDCard |
Yes | |
|
UART |
Soon | |
| Ethernet | Yes |
2 ports (only 1 port on J6Eco)
|
The board can boot either SDCard or eMMC. SDCard only on IDK - See more at: