I have measured a significant difference (6x) between the back-up clock current when configured and when not configured or configured improperly. When not configured, it draws more current and I'm curious if this is an appropriate steady-state condition or should safeguards be built in to prevent continued powering of the RTC circuit when the clock is not configured.
Thanks,