This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

McBSP activity, but no RRDY

What would cause RRDY not to go high when there is good line activity on the McBSP?

Details : I'm using McBSP0, and generating CLKR and FSR.  I open my McBSP, configure it, and start it.  I see nice CLKR and FSR waveforms reading my ADC.  I see data on DSR coming from my ADC.  My logic analyzer decodes it nicely.  Yet RRDY never goes high!  When I call the following function, it hangs on the while() loop forever.

 

Uint32 MCBSP_sentry_read32( MCBSP_Handle hMcbsp ){

    // Wait for read to be ready

    while( ! MCBSP_rrdy( hMcbsp ) );

    // Read it in

    return MCBSP_read32( hMcbsp );

}

 

I configure it like so...

jj_test_config.spcr1 = 1 << 13; /* Sign extend and right-justify */ 

        jj_test_config.spcr2 = 1 << 9 | 3 << 6;  /* Sample rate generator enabled.*/

        jj_test_config.xcr1 = 0;

        jj_test_config.xcr2 = 0;

        jj_test_config.rcr1 = 5 << 5; /* Received word length... 32 bit transactions */

        jj_test_config.rcr2 = 1 << 2 | /* Frame sync error ignore. */ 

                              1;        /* 1 Bit of data delay.  Data starts clock after the FS. */

        jj_test_config.srgr1 = 23;     /* CLKDVG of 23 */

        jj_test_config.srgr2 = 1 << 13 | /* CLKSM = 1 for internal McBSP clock*/

                               33;      /* FPER of 34 - 1*/

        jj_test_config.pcr = 0x0F00; //1 << 10 | 1 << 8; // | 1 << 2;   /* Turn on Frame sync from internal.  DRCLK driven out..*/  

mhMcbsp = MCBSP_open( MCBSP_PORT0, MCBSP_OPEN_RESET );

MCBSP_config( mhMcbsp, &jj_test_config ); MCBSP_start( mhMcbsp, MCBSP_RCV_START | MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC, 33 ); // Turn on interrupts globally IRQ_globalEnable();

 

Then I just read it in a loop, but RRDY is never high?  What's broken here?  Am I missing some subtlety?

 

Thanks.