This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm6437 jpeg encoder demo

I am trying to run the jpeg encoder demo TestAppEncoder on a custom dm6435 board.  Board hardware should be fine, I have run multiple other projects on it and I have confirmed that it has enough ddr2 memory attached for the new project.  I have successfully built and started running the project, but the code is hanging "forever" (at least several minutes so far) in the function call to TestApp_ReadInputData().  Further, it never returns from the fread call inside.  I have tried rebuilding the project with the rts46plus library instead of the original rts6000 in the project settings, but I get the same behavior.  Here is my standard out prior to the hang:

 

*******************************************

Read Configuration Set 1

*******************************************

Running in Compliance Mode

 Input file...  ..\..\Test\TestVecs\Input\remi003_422.yuv  

Test File... ..\..\Test\TestVecs\Reference\remi003_422.jpg

Creating Algorithm Instance...

Algorithm Instance Creation Done...

 

Is there anything that I'm missing in getting this demo to run on the 6435?